STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

HAL_UART_DMA_Pause() does not pause the UART receiving bytes

Hi allI'm using a Nucleo U575 board for reading a GNSS module. I configured the USART2 port with DMA (in circular mode, port 0 as it's peripheral to memory), Request is USART2_RX, Interrupts for USART2 and GPDMA1 are enabled and it works just fine. I...

MGuth.1 by Associate III
  • 1853 Views
  • 1 replies
  • 0 kudos

Resolved! G030 temperature sensor results (very) inaccurate

Hello all,I am trying to read temperature with the G030. At the moment there is quite a large difference between actual temperature and temperature read by the MCU (true temperature around 23.5 degC while MCU reads 32 degC)ADC_Init code:static void A...

ZJing by Associate III
  • 3946 Views
  • 9 replies
  • 1 kudos
DJ1 by Associate III
  • 3905 Views
  • 1 replies
  • 0 kudos

Question abut stm32u5 internal flash

Hi,The stm32u5's internal flash has feature "10 kcycles endurance on all Flash memory. 100 kcycles on 256 Kbytes per bank".Please advise the memory address of "100 kcycles on 256 Kbytes per bank".Thanks,QiZhang

zqizh.1 by Associate III
  • 4735 Views
  • 11 replies
  • 0 kudos

Getting huge different Delay time in measuring a blocking delay timer which run in different memory address of STM32H7a3ii. Was this behavior of the MCU?

I create a simple blocking delay timer using simple looping and run in STM32H7a3ii. The program was linear, no code optimization, no interrupt. Without any changes of the blocking delay timer function, i found that when the blocking delay timer place...

WChan.5 by Associate II
  • 5565 Views
  • 11 replies
  • 0 kudos

Resolved! STM32G030K6T6 oscillator pins

As per datasheet pin 2 and pin 3 are OSC32_IN and OSC32_OUT pins I want to connect a 8MHZ crystal and was looking for OSC_IN and OSC_OUT pins, but could not find any info regarding them, can the OSC32_IN and OSC32_OUT pins be used for connecting the ...

0693W00000bhMAbQAM.png
MMala.3 by Associate II
  • 3160 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.