2017-11-06 2:55 PM
I'm setting up a UART channels to transmit and receive from a slave device.
I have Transmit working as I can see the slave is doing what's asked from the command sent to it.
On each command the slave reply's back with acknowledgement.
When I capture the ACK I get HAL_Timeout
Example
static uint16_t timeout = 25; // milliseconds
static HAL_StatusTypeDef val_tx1, val_tx2; static HAL_StatusTypeDef val_rx1, val_rx2;val_tx1 = HAL_UART_Transmit_DMA(&huart1, buffer, buff_size);
val_rx1 = HAL_UART_Receive(&huart1, rcv1_msg, rcvmsg1_size, timeout);while (HAL_UART_GetState(&huart1) != HAL_UART_STATE_READY){}
The execution is stuck forever in the while loop since the HAL UART state is HAL_TIMEOUT
I actually want to use UART Receive with interrupt which fills the RX buffer and I want to simply parse thru the buffer.
But when I use HAL_UART_Receive_IT() the return is always HAL_UART_STATE_BUSY_RX.
How do I go about fixing this.
Thanks.
#uart-tx #uart-rx #uart-it #stm32-usart #usart-stm322017-11-06 4:21 PM
May be you should be testing the return of
HAL_UART_Receive(), and states other than READY?
A receive timeout may occur if the sending device hasn't sent data within the window you are expecting. You could make the timeout longer, or resubmit the request.
2017-11-07 1:03 PM
Hello Clive,
Thanks for your response.
The return of HAL_UART_Receive() is HAL_OK for the first time around and then always HAL_TIMEOUT which means I'm not setting up my RX properly. On an oscilloscope I can see acknowledgement from the slave device for every command I send. I have given HAL_UART_Receive() sufficient timeout. But as I mentioned I would prefer to use HAL_UART_Receive_IT() instead since I want to generate an interrupt and execute its routine when I receive acknowledgement. How would I go about setting up interrupt?
Some Correction to the code I had provided in my first post...here is something what I'm trying to do.
static uint16_t timeout = 25; // milliseconds
static HAL_StatusTypeDef val_tx1;static HAL_StatusTypeDef val_rx1;while(1)
{
val_tx1 = HAL_UART_Transmit_DMA(&huart1, buffer, buff_size);
val_rx1 = HAL_UART_Receive(&huart1, rcv1_msg, rcvmsg1_size, timeout);while (HAL_UART_GetState(&huart1) != HAL_UART_STATE_READY){}
// more code here to modify buffer and buff_size to transmit new command to slave device
}
Thanks.
2017-11-07 2:10 PM
Ok, but not testing for results, and no handling of appropriate loop exit conditions...
HAL_UART_Transmit_DMA() will complete immediately, before the data has been sent, so the timeout is going to need to include the transit time of the outbound data.
HAL_UART_Receive() will block.
2018-07-07 7:34 AM
Did you manage to fix this problem? I'm stuck on this too.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.