2018-05-07 2:02 PM
I am using HAL I2C to interface Cryptomemory (from ATMEL). Using I2C master transmit(HAL_I2C_Master_Transmit_DMA), I need to differentiate the following two conditions of device,
1. Send B4+ACK, 00+ACK, 00+ACK, 01+NAK
2. Send B4+NAK
They are both valid operations in this device under certain conditions. In the second condition, I need to repeat sending B4 until ACK received.
I wasn't able to differentiate using HAL_I2C_GetError because both return the same error. Is there a way to know DMA queue transferred count?
If not possible, I might need to abandon DMA.
Thanks.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.