2023-07-25 5:21 AM
Hi,
I have several programm where I use either the HAL_FLASH_Program command or some EEPROM command like EE_ReadVariable16bits (directly issued from the std "eeprom_emul.h" library).
To make those command functionnal i had to stop the watchdog which triggering even if I increase the time to some higher values (I have prescaler = 256, and reload = 1000 thus having a 8s delay ...)
Do you what could the issue to make both working together ?
thanks,
Edgar
2023-07-25 5:38 AM - edited 2023-07-25 5:39 AM
Depending on the part, and the size of the blocks chosen, the erase can take multiple seconds. The MCU will stall if you try to interact with the FLASH whilst it is busy.
You'd need to move all the code the MCU is expected to execute into RAM (including vector tables, interrupt handlers, etc)
Add a real EEPROM, or QSPI NOR Flash, Rethink your use/mechanics for saving things this way, vs NVRAM
2023-07-25 7:43 AM
Hi !
I don't think the time is the issue as the HAK_FLASH_PROGRAMM doesn't take long (mesured around 10ms.)
So the watchdog shall not trigger (8s) .
I could break everything to move code to other places but I don't really get why this would change the behaviour.
Thank you for your explanations,
Edgar
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.