2015-05-20 8:13 AM
Hi,
I am using the HAL driver for the CAN interface of an STM32F207. I noticed that the payload data in the current driver for the F2 is unneccessarily defined as arrays of uint32_t. In the current release for the STM32F4 this was changed to uint8_t. This change is also mentioned in the release notes for the STM32F4. For the F2 no new releases were published for over a year. Will there be any new releases for the F2 or has ST stopped support? I have already contacted ST on this but no answer so far. Regards, Ralph2015-05-22 3:35 AM
Hello Christopher,
I confirm that STM32CubeF2 still being supported. A new release will be available soon to be aligned with other packages and fix some issues.-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2015-05-26 1:49 AM
Hi Mayla,
can you give a date on this? Will it be weeks, months, years? I have to decide if I want to code around the bugs or wait for the new release. If it takes longer, I will need a list of known bugs. I guess I am not the only one. Ralph2015-05-26 11:49 AM
Always assume you're on your own, and plan accordingly.
The F4 and F2 parts are *very* similar on the peripheral side. Your most effective course of action would be to merge/diff the pieces/examples you're most concerned with.2015-09-01 12:46 PM
Hi Mayla,
we want to use STM32F207 for our new project, but HAL driver is very old.When
will be available a new release ? PetrWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.