2023-04-16 3:53 AM - edited 2023-11-20 8:04 AM
So I've created a project and am trying to use the HAL_delay(10); but it gets stuck at this function when im trying to debug.
I have been changing the clock and enabling the TIM2 so I don't know if i've messed something up. Here are the settings that I have:
And that is about it
2023-04-18 3:11 AM
i was thinking, HAL_Delay() is working - just you cannot debug it...
so: because program is running (you said ) , test : with simmple LED toggle...is there delay or not ?
2023-04-18 3:13 AM
I thought I should be able to debug it eitherway. Will try with LED
2023-04-18 3:57 AM
Okay so I tried with the LED and found out that the program doesn't really run. Didn't even get to the first PIN_SET without debuging step by step
2024-11-19 1:18 AM
I am having the same problem and my HAL_Delay is not working either. I thought I would find the solution here. You didn't find it either.
2025-05-08 10:07 AM
The debug is the problem. Systick stop working during a debug-session. Since my app is a single thread I replaced every HAL_Delay with a normal loop with some NOP() that made up a delay_1us()....
I haven't found a solution to this problem. To much work when it can be solved with a simple loop.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.