2024-03-13 6:10 AM - edited 2024-03-13 6:10 AM
Hi,
i was hoping, that the Link-V3 would just work, after i used nucleo boards already. But i was dissapointed. I use the GDB server, and it says:
ST-Link enumeration failed
Error in initializing ST-LINK device.
Reason: ST-LINK DLL error.
I just checked a Nucleo board, and there is no problem.
The installation of the driver worked without errors.
Solved! Go to Solution.
2024-03-13 11:33 PM
2024-03-13 11:38 PM
2024-03-14 12:28 AM
I now managed to get some connection to my board. I used the Cubeprogrammer GUI, and have to set 1000kHz or lower. But still it does not work with the CLI, allthough it there set 1000kHz too.
2024-03-14 12:51 AM
IT WORKS!
While trying many things, i disconnectes NRST. But i still can program the target.
I had to enter the frequency in the gdb server comman line!
2024-03-14 8:28 AM
TARGET - the thing you're trying to communicate / connect too..
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.