2019-05-10 4:34 AM
Hello Everyone,
I am trying to interface MPU6050 with STM32L072Z and while communicating to I2C line I am always getting constant value, bellow is the code
void Serialprint(char *msg)
{
uint16_t msg_len = strlen(msg);
HAL_UART_Transmit(&huart2, (uint8_t*)msg , msg_len, 10U);
}
long accelX, accelY, accelZ;
HAL_I2C_Mem_Write(&hi2c2,0x68<<1,0x6B,sizeof(uint16_t),buffer,2,10U);
HAL_Delay(100);
HAL_I2C_Mem_Write(&hi2c2,0x68<<1,0x1B,sizeof(uint16_t),buffer,2,10U);
HAL_Delay(100);
HAL_I2C_Mem_Write(&hi2c2,0x68<<1,0x1C,sizeof(uint16_t),buffer,2,10U);
HAL_Delay(100);
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
while((HAL_I2C_Mem_Read(&hi2c2, 0x68<<1,0x3B,sizeof(uint16_t),buff,6,10U)) != HAL_OK)
{
Serialprint("ERROR");
}
accelX = buff[0]<<8|buff[1]; //Store first two bytes into accelX
accelY = buff[2]<<8|buff[3]; //Store middle two bytes into accelY
accelZ = buff[4]<<8|buff[5];
// accelX = accelX /16384;
// accelY = accelY /16384;
// accelZ = accelZ /16384;
sprintf(ax, "%d",accelX);
sprintf(ay, "%d",accelY);
sprintf(az, "%d",accelZ);
Serialprint("AX : ");
Serialprint(ax);
Serialprint("\n\r");
Serialprint("AY : ");
Serialprint(ay);
Serialprint("\n\r");
Serialprint("AZ : ");
Serialprint(az);
Serialprint("\n\r");
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.