2014-03-01 2:52 AM
Hi,
I want to generate a timer interrupt for 6.25 us, 9.375 us, 0.1 milisec, 0.4 millisecond and so on . I think that it can be done by using DMA taking the array SRC_Buffer_DEC[4] ={200,300,3200,12800} as DMA memory base address and ADC1->ARR as peripheral address therefore the Auto reload value should change everytime and should generate an interrupt for each value. but I am not able to do that . I didn't get any example for this but I think that it can be done. Can anybody help me and say me whether my thinking is right or wrong. whether it is achieveable, if no how it can be done? I have paste my code below please see #include ''unistd.h'' #include ''stm32f4xx.h'' #include ''stm32f4_discovery.h'' #include ''stm32f4xx_tim.h'' #include ''stm32f4xx_rcc.h'' #include ''stm32f4xx.h'' #include <misc.h> #include ''stm32f4xx_adc.h'' #include ''stm32f4xx_gpio.h'' #include ''stm32f4xx_dac.h'' #include ''stm32f4xx_tim.h'' #include ''stm32f4xx_dma.h'' #include ''stm32f4xx_usart.h'' #include ''time.h'' uint16_t SRC_Buffer_DEC[4] ={200,300,3200,12800}; int main(void) { STM_EVAL_LEDInit(LED3); rcc(); INTTIM_Config(); NVIC_Configuration(); EnableTimerInterrupt(); while(1); DMA(); #ifdef DEBUG debug(); #endif } void rcc() { RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_DMA1, ENABLE); /** * Enable clock for DMA2 (ADC DMA) **/ RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_DMA2, ENABLE); /** * Enable clock for TIM2 (used for ADC Trigger) **/ RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE); } #if 1 void DMA() { DMA_InitTypeDef DMA_InitStructure; DMA_InitStructure.DMA_Channel = DMA_Channel_6; DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)&TIM2->ARR; DMA_InitStructure.DMA_Memory0BaseAddr = (uint32_t)&SRC_Buffer_DEC; DMA_InitStructure.DMA_DIR = DMA_DIR_MemoryToPeripheral; DMA_InitStructure.DMA_BufferSize = 4; DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable; DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable; DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord; DMA_InitStructure.DMA_MemoryDataSize = DMA_PeripheralDataSize_HalfWord; DMA_InitStructure.DMA_Mode = DMA_Mode_Circular; //DMA_InitStructure.DMA_Mode = DMA_Mode_Normal; DMA_InitStructure.DMA_Priority = DMA_Priority_High; DMA_InitStructure.DMA_FIFOMode = DMA_FIFOMode_Disable; DMA_InitStructure.DMA_FIFOThreshold = DMA_FIFOThreshold_Full; DMA_InitStructure.DMA_MemoryBurst = DMA_MemoryBurst_Single; DMA_InitStructure.DMA_PeripheralBurst = DMA_PeripheralBurst_Single; DMA_Init(DMA2_Stream4, &DMA_InitStructure); // DMA_ITConfig(DMA2_Stream4, DMA_IT_TC | DMA_IT_HT, ENABLE); DMA_Cmd(DMA2_Stream4, ENABLE); /* TIM8 Update DMA Request enable */ TIM_DMACmd(TIM2, TIM_DMA_Trigger , ENABLE); TIM_DMACmd(TIM2, TIM_DMA_Update, ENABLE); } #endif void INTTIM_Config(void) { TIM_TimeBaseInitTypeDef TIM_InitStruct; TIM_OCInitTypeDef TIM_OCInitStructure; /* TIM2 clock enable */ /* Time base configuration */ TIM_InitStruct.TIM_Prescaler = 2 - 1; // This will configure the clock to 2 kHz TIM_InitStruct.TIM_CounterMode = TIM_CounterMode_Up; // Count-up timer mode // TIM_InitStruct.TIM_Period = 200 - 1; // 2 kHz down to 1 Hz = 1 second TIM_InitStruct.TIM_ClockDivision = TIM_CKD_DIV1; // Divide clock by 1 TIM_InitStruct.TIM_RepetitionCounter = 0; // Set to 0, not used TIM_TimeBaseInit(TIM2, &TIM_InitStruct); TIM_ARRPreloadConfig(TIM2, ENABLE); /* TIM8 enable counter */ TIM_Cmd(TIM2, ENABLE); /* TIM2 enable counter */ TIM_ITConfig(TIM2, TIM_IT_Update, ENABLE); } void EnableTimerInterrupt() { NVIC_InitTypeDef nvicStructure; nvicStructure.NVIC_IRQChannel = TIM2_IRQn; nvicStructure.NVIC_IRQChannelPreemptionPriority = 0; nvicStructure.NVIC_IRQChannelSubPriority = 0; nvicStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&nvicStructure); } void TIM2_IRQHandler() { if (TIM_GetITStatus(TIM2, TIM_IT_Update) != RESET) { TIM_ClearITPendingBit(TIM2, TIM_IT_Update); STM_EVAL_LEDToggle(LED3); } }2014-04-10 9:07 AM
That's a relief, because I did test it.
2014-04-29 12:35 AM
2014-04-29 5:02 AM
Perhaps that you don't enable it in the NVIC?
NVIC_InitTypeDef NVIC_InitStructure;
/* Enable the TIM3 gloabal Interrupt */
NVIC_InitStructure.NVIC_IRQChannel = TIM3_IRQn;
NVIC_InitStructure.NVIC_IRQChannelPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);
2014-04-29 5:55 AM
Hi clive It's working but it's working for only timer 3 timer 15 , 16 and 17 it's not able to generate the interrupt I am not getting it why . I have checked the DMA channel , channel 5 for TIM15_UP , Channel 1 and channel 4 for timer TIM17_UP and TIM16_UP respectively . Why is it so
2014-04-29 5:59 AM
2014-04-29 6:26 AM
Why is it so
Do you have the right startup_stm32f03xxxx.s file in the project? Does it describe the vectors you are attempting to use?2014-04-29 6:53 AM
Hi
I didn't get it........can you please explain2014-04-29 7:08 AM
I didn't get it........can you please explain
Read the words again slowly, and think harder.2014-04-29 10:30 PM
2014-04-30 6:50 AM
void TIM3_IRQHandler(void) ??
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.