2019-05-09 11:27 PM
Hello, maybe it's not the right place to ask this type of questions, in case I apologize.
While trying to understand how ARM assembler works, I came across this problem and I'm currently struggling to find the answer.
Before explaining better my question what I want to do is to know the exact value of the instruction pointer of a certain instruction X, at runtime and without resorting to the debugger. I want to monitor the address of certain isntructions by sending it to an external tool, so I want to know, if I use the below code, which are the adjustment (if any) to the value of R1 in order to contain the address of the instruction X.
This is what I thought to acomplish this task:
MOV R1,PC
ADD/SUB R1, something ;if some adjustment is required
X ; instruciton I want to monitor
;send R1 to an external componentI cannot quite understand which is the rule about the value of PC, I found that is + 4 or +8 depending on if it is Thumb or ARM instruction but it seems that this rule is not always followed. Since I'm working on a cortex-M4 (STM32f429) only Thumb instruction are supported
I try to explain better with some example
If I analyze this code:
80001d0: b508 push {r3, lr}
80001d2: 4b03 ldr r3, [pc, #12]
80001d4: b11b cbz r3, 80001de
80001d6: 4903 ldr r1, [pc, #12]
80001d8: 4803 ldr r0, [pc, #12]
80001da: f3af 8000 nop.w
80001de: bd08 pop {r3, pc}
80001e0: 00000000 .word 0x00000000
80001e4: 2000000c .word 0x2000000c
80001e8: 0800328c .word 0x0800328cI found that in the first ldr pc is equal to the function pointer +2
in the second ldr also the value of pc is the function pointer +2, but in the last ldr pc is equal to the function pointer +4 (and is what that i'm expecting to appen in every case, if i've understood correctly).
Hope to been clear enough on which is my problem.
Thank you for your time, hope you can help me in some way
Best regards
2019-05-10 1:19 AM
Thumb-2 has both 16-bit and 32-bit instructions, that's why you see either +2 or +4 bytes.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.