2012-06-08 2:56 PM
Hello all,
I am using stm32f217 on my target board. it has a mutiplexed 8MB psram. My problem is my one 16bit write changes the value written by previous 16bit write. write_ram16(0,0xaaaa)-->16 bit write at offset 0, base add 0x60000000 write_ram16(2,0xf000) read_ram16(2) --> returns 0xf000 read_ram16(0) -->returns 1 my fsmc config is FSMC_Bank1->BCR1 = (FSMC_BCR_MBKEN | //bank enable FSMC_BCR_MTYP_PSRAM | //memory is psram FSMC_BCR_MWID_16BITS |//16bit wide FSMC_BCR_WREN | //write enable FSMC_BCR_MUXEN); //mux enable FSMC_Bank1->BTR1 = 0x00010401; //DataSetupTime = 4, BusTurnAroundDuration = 1, add setup=12012-06-08 11:50 PM
would be good if you can provide the Schematics for review.
Better to use the Fw library example on FSMC2012-06-09 4:14 AM
Hello alokm,
i think in the FW library example, the ram is connected in non multiplexed way. is it right or is there any example where ram is connected in multiplexed way also? attached are the gpio and sram schematics ________________ Attachments : gpio.bmp : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtUW&d=%2Fa%2F0X0000000aQl%2FPi3cW8s7QgKKBllhaVpZUrVfUeiYrLOwsnwWEvSgr4o&asPdf=falsesram.bmp : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtUb&d=%2Fa%2F0X0000000aQm%2F8Msf1nrrcyE2BDIYP.KZj1GDq4RrJKFydn3T76iznK8&asPdf=false2012-06-11 6:41 AM
Hi,
according to you , You are reading the same data as you have written in the last. can you explain the following function write_ram16() & read_ram16().There may be error in address handling . Regards Balmukund prasad2012-06-12 6:16 PM
from the schematics, nothing seems wrong. Can you change the FSMC settings to allow more time for RAM to setup the data on data bus ? maybe it's timing problem.
i am not aware of any schm of mux-ed ram. there do exist an AN on FSMC, not sure if it talks about the mux mode of fsmc2012-06-13 12:33 PM
Hello Prasad,
read and write functions are quite straightforward. below is the implementation. uint16_t read_ram16(uint32_t offset) { volatile uint16_t * t=(0x60000000+offset); return *t; } void write_ram16(uint32_t offset,uint16_t data) { volatile uint16_t * t=(0x60000000+offset); *t = data; }2012-07-01 11:15 AM
You are wrong in schematics. NL line should be inverted. Otherwise (as in you case) you'll see a latched data instead of RAM content (and RAM content differs from that you may expect).
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.