2014-09-22 7:21 AM
hey all,
i am using STM32F4 MCU. trying to connect LCD controller (ILI9342C) using FSMC.i understand that i can use the 8 bit bus.how can i determine which bus to use : D0-D7 or D8-D15Thanx #fsmc2014-09-22 8:35 AM
On the STM32 side or the LCD Controller side.
From the STM32 D8..15 would only be present if you used at 16-bit bus, and shifted the data into the high order byte The key difference in 16-bit mode is that the sense of A0, and other address bits, is shiftedWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.