2018-06-18 2:53 AM
Hello,
We are trying to command a BLDC motor using the FOC lib 4.3 and we notice the following behavior:
- When the brake is activated (mechanical braking system) the motor is totally blocked and dose not start up even after releasing the brake.- When the brake is deactivated before starting up the system, the motor works properly.The brake is a mandatory for our system so:
- Is it possible to change the rotation direction of the alignment at start up?- Is it possible to avoid using the alignment functions?Thank you.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.