2016-04-14 3:42 AM
Hi all
Assume that I have SDRAM 13rowx10col is connected to stm32f7.
I need to know the order of rows in conjunction with banks. Is physical address is calculated as follows: A12 A11 A10 A9 A8 A7 A6 A5 A4 A3 A2 A1 A0 BA1 BA0 or so: BA1 BA0 A12 A11 A10 A9 A8 A7 A6 A5 A4 A3 A2 A1 A0 Assume address 0xC2000000 or 0x2000000 / 10bit cols = 0x8000 row, the row (and bank) address = 100000000000000b So this will be significant bit BA1 or A12? in pdf: http://www.nxp.com/documents/application_note/AN10935.pdf on page 16we see that the bank is the lowest.
But as is in FMC? [Edit]I will add
that I have crosstalk on memory buss. The lower 32 MB memory works fine.While the upper
32MB
memory has errors. I suppose that it is a track A12 which isin one place
too close to the
SDRAM clock. But I know if I am right that the banks are lower. Thanks #sdram-fmcWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.