2018-01-30 2:14 AM
Hello.,
I am working on STM32F7 microcontroller , need to access external memory device through parallel bus (8 bit bus width). The external memory doesn't support RDY signal so that I need to add internal wait state , But I don't find which parameter need to set add internal wait state.
Can anyone suggest me which register I need to configure.
Presently I configure FMC controller as fallows ;-
hnor1.Instance = FMC_NORSRAM_DEVICE;
hnor1.Extended = FMC_NORSRAM_EXTENDED_DEVICE; /* hnor1.Init */ hnor1.Init.NSBank = FMC_NORSRAM_BANK4; hnor1.Init.DataAddressMux = FMC_DATA_ADDRESS_MUX_DISABLE; hnor1.Init.MemoryType = FMC_MEMORY_TYPE_NOR; hnor1.Init.MemoryDataWidth = FMC_NORSRAM_MEM_BUS_WIDTH_8; hnor1.Init.BurstAccessMode = FMC_BURST_ACCESS_MODE_DISABLE; hnor1.Init.WaitSignalPolarity = FMC_WAIT_SIGNAL_POLARITY_LOW; hnor1.Init.WaitSignalActive = FMC_WAIT_TIMING_BEFORE_WS; hnor1.Init.WriteOperation = FMC_WRITE_OPERATION_ENABLE; hnor1.Init.WaitSignal = FMC_WAIT_SIGNAL_DISABLE; hnor1.Init.ExtendedMode = FMC_EXTENDED_MODE_ENABLE; hnor1.Init.AsynchronousWait = FMC_ASYNCHRONOUS_WAIT_DISABLE; hnor1.Init.WriteBurst = FMC_WRITE_BURST_DISABLE; hnor1.Init.ContinuousClock = FMC_CONTINUOUS_CLOCK_SYNC_ASYNC; hnor1.Init.WriteFifo = FMC_WRITE_FIFO_ENABLE; hnor1.Init.PageSize = FMC_PAGE_SIZE_NONE; /* Timing */ Timing.AddressSetupTime = 15; Timing.AddressHoldTime = 15; Timing.DataSetupTime = 255; Timing.BusTurnAroundDuration = 15; Timing.CLKDivision = 16; Timing.DataLatency = 17; Timing.AccessMode = FMC_ACCESS_MODE_A; /* ExtTiming */ ExtTiming.AddressSetupTime = 15; ExtTiming.AddressHoldTime = 15; ExtTiming.DataSetupTime = 255; ExtTiming.BusTurnAroundDuration = 15; ExtTiming.CLKDivision = 16; ExtTiming.DataLatency = 17; ExtTiming.AccessMode = FMC_ACCESS_MODE_A;Thank you.,
#parallel #fmc #stm32f765bitWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.