2023-11-16 2:24 PM
Does the STM32G0 with the CMSIS libraries support floating point operations?
Is the G0 recommended for floating point operation, or should I use the F1 series instead?
Thank you!
Solved! Go to Solution.
2023-11-25 9:44 AM
Think through the math and the range of numbers at each stage of the computation, perhaps scale or used fixed point representations.
Get a device that will hold enough of the float library, a 16 KB Flash device is going to be a bit tight to do much, but the G0 and C0 parts come in some larger capacities.
2023-11-16 2:46 PM
The Cortex-M0(+) uses software libraries for floating point, so does the Cortex-M3
On the M4F some simple operations are facilitated in hardware on the single-precision FPU
How much math and the precision will determine if 64 MHz operation is sufficient.
2023-11-24 11:23 AM
Thank you. Can you recommend a reference about algorithm implementations with integers only, not floating point?
2023-11-25 9:44 AM
Think through the math and the range of numbers at each stage of the computation, perhaps scale or used fixed point representations.
Get a device that will hold enough of the float library, a 16 KB Flash device is going to be a bit tight to do much, but the G0 and C0 parts come in some larger capacities.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.