2021-08-05 5:48 PM
Hi All,
I cannot figure out why the series of instructions below is not working for me (device is a STM32F303x6).
This is just me fiddling around getting to know the CPU, I have this setting so the FP opcodes are accepted by the compiler, and it seems to be compiling what I do just fine.
.fpu fpv4-sp-d16
I have enabled the Floating Point Co-Processor as specified in the Cortex-M4 programmers manual (PM0214): Set bits 20-23 in CPACR.
But still the code below does nothing with the 's' registers.
movw r4, #4096 // Put a test value into r4
vmov s15, r4 // Copy r4 value into s15 Flt register for conversion to float
vcvt.f32.u32 s15, s15, #32 // Convert s15 'U32 value 4096' to f32 (result should be s15 = 0x45800000)
When I look at the s15 register values (in STM32CubeIDE) when debugging the code it never changes, the transfer of the value from r4 doesn't even seem to happen.
I can't see what I am doing wrong for the value to never be transferred in to the floating point register. Anyone traveled this road before? I'm hoping I just forgot to set something else up in the CPU.
Thanks.
Solved! Go to Solution.
2021-08-05 7:04 PM
Try moving it back to a processor register, like R0 and return from a subroutine
This gets me 0x35800000 (0.000000954)
vcvt.f32.u32 s15, s15, #32
This gets me 0x45800000 (4096.0)
vcvt.f32.u32 s15, s15
Did this in Keil
fputest
export fputest
movw r3, #4096 ; Put a test value into r4
vmov s15, r3 ; Copy r4 value into s15 Flt register for conversion to float
vcvt.f32.u32 s15, s15 ;, #32 ; Convert s15 'U32 value 4096' to f32 (result should be s15 = 0x45800000)
vmov r0, s15
bx lr
2021-08-05 7:04 PM
Try moving it back to a processor register, like R0 and return from a subroutine
This gets me 0x35800000 (0.000000954)
vcvt.f32.u32 s15, s15, #32
This gets me 0x45800000 (4096.0)
vcvt.f32.u32 s15, s15
Did this in Keil
fputest
export fputest
movw r3, #4096 ; Put a test value into r4
vmov s15, r3 ; Copy r4 value into s15 Flt register for conversion to float
vcvt.f32.u32 s15, s15 ;, #32 ; Convert s15 'U32 value 4096' to f32 (result should be s15 = 0x45800000)
vmov r0, s15
bx lr
2021-08-05 7:18 PM
Thanks, that does the same for me as well (result ends up as 0x35800000 when I move it back out of the s15 register).
As I stepped through the code I never saw the s15 register change though, maybe that is just how it is.
But thanks, at least I know now if I want to 'see' the result on screen I can just vmov the result out to a normal register.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.