2021-01-25 1:26 AM
Dear ST Hello,
I have a big problem with floating point calculations,
I am trying to implement the IIR filter to filter a current but the result is Zero.
Sometimes the watch expression window shows me 0 but the input filter is not zero.
/* Get the HImax */
HimaxCurrentCons = HAL_ADC_GetValue(&hadc2);
/* Get LSM current */
l_u16AdcCurrent = HAL_ADC_GetValue(&hadc1);
/* Filter the current LSM */
Input[0] = (float_t)1E6;//l_u16AdcCurrent;
filter_out = FilterCoefInput[0] * Input[0];
for (int i = 6; i > 0; i--)
{
/* adding the ai * xi i=7..1 */
filter_out = filter_out + (FilterCoefInput[i] * Input[i]);
/* Shifting the register input */
Input[i] = Input[i - 1];
}
for (int j = 6; j > 0; j--)
{
/* Adding the bj * yj j = 6..1 */
filter_out = filter_out + (FilterCoefOutput[j] * Output[j-1]);
/* Shifting the register output */
Output[j] = Output[j - 1];
}
Output[0] = filter_out;
/* Current compute */
LsmCurrent = (300.0/2559) * filter_out;Thank in advance,
S.tarik
2021-01-25 1:59 AM
What MCU? And: you are not showing all types.
2021-01-25 2:02 AM
I am using the STM32F407 discovery board,
const float_t FilterCoefInput [7] = {
#if IMPULS
8.576557E-06f, 5.145934E-05f,
1.286483E-04f, 1.715311E-04f,
1.286483E-04f, 5.145934E-05f,
8.576557E-06f
#else
8.576557, 51.45934,
128.6483, 171.5311,
128.6483, 51.45934,
8.576557
#endif
};
const float_t FilterCoefOutput [7] = {
#if IMPULS
1.0f, +4.787135f,
-9.6495177f, +10.46907f,
-6.44111188f, +2.129038f,
-0.2951724f
#else
1.0f, +4.787135f,
-9.6495177f, +10.46907f,
-6.44111188f, +2.129038f,
-0.2951724f
#endif
};
float_t Input[7] = {0.0};
float_t Output[6] = {0.0};
float_t filter_out = 0.0f;I am trying different configurations to solve this problem,
thank you
2021-01-25 2:26 AM
You define:
> Output[6]
but in the loop you write to Output[j] when j == 6.
JW
2021-01-25 2:27 AM
If Output array has size 6, the first write to Output[j] with j=6 is illegal, potentially overwriting filter_out. Make the array larger.
2021-01-27 4:55 AM
Thank you,
that was the problem
2021-01-27 4:56 AM
yes JW, thank you for help.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.