2020-01-16 9:38 AM
Dear all ,
I know that this is the ridiculous questions with engineers here, but i still have to ask because i really don't know. Pease forgive for me if this type of questions were already answered in another topic.
I'm using STM32F100 to design the PCB, almost boards that i refer i saw Boot pins are connected to the jumper to select the boot mode. But i don't intend to flash the software via USART , USB..., i want to use ST-Link , because i'm able to debug the SW. Therefore, my question is that do i have pull up / down the Boot pins, or just keep it open as not using.
Thank you in advance!
Solved! Go to Solution.
2020-01-16 9:44 AM
You should pull BOOT0 down to ensure it runs your software from FLASH every time it starts, leaving it floating can be problematic if your supply has a slow rise time.
With BOOT0=LOW, BOOT1 is DON'T CARE
2020-01-16 9:44 AM
You should pull BOOT0 down to ensure it runs your software from FLASH every time it starts, leaving it floating can be problematic if your supply has a slow rise time.
With BOOT0=LOW, BOOT1 is DON'T CARE
2020-01-16 9:48 AM
Wow, thank you very much.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.