2022-02-18 9:47 AM
2022-09-23 6:39 AM
Hello @AShel.1,
For read/write NOR flash using FMC interface, you can check the examples provided within the STM32Cube_FW.
For instance the one on the STM32L476G-EVAL, you can find it under the "...\STM32Cube_FW_L4_V.XX\Projects\STM32L476G-EVAL\Examples\FMC\FMC_NOR" root.
To get quick technical support on further threads, I advise you to provide detailed description concerning your question/problem, the setup you are working with, etc..
Thank you.
Chahinez.
2022-02-18 12:07 PM
What thread?
The MTP plumbing would presumably go to an underlying file system.
2022-02-18 10:27 PM
I'm using FMC mechanism
2022-02-21 8:38 AM
I'm using FMC
2022-09-23 6:39 AM
Hello @AShel.1,
For read/write NOR flash using FMC interface, you can check the examples provided within the STM32Cube_FW.
For instance the one on the STM32L476G-EVAL, you can find it under the "...\STM32Cube_FW_L4_V.XX\Projects\STM32L476G-EVAL\Examples\FMC\FMC_NOR" root.
To get quick technical support on further threads, I advise you to provide detailed description concerning your question/problem, the setup you are working with, etc..
Thank you.
Chahinez.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.