2018-07-08 3:58 AM
I'm trying to debug a project in TrueStudio, but get this error message during flashing:
... which is the ''load'' instruction of the startup script.
I think the cause of this error is, that the flash size of my program can't be divided by 4 without remainder:
Print size information
text data bss dec hex 132474 640 38232 171346 29d52If I modify the project by inserting a while(1) before the use of the library, which makes the flash size not a multiple of 4 bytes, it can be flashed.
Console output:
Flash write: Address= 0x800d0a8, Length=70
Programming flash.. STM32 device: flash programming successful 0x800d0a8 Flash write completed in 0.085000 seconds, 0.804228kB/sFlash write: Address= 0x800d0ee, Length=126 Programming flash.. Flash programming alignment errorI ported this project from an F3 MCU to the L4 MCU. The F3 project could be flashed by TrueStudio without any problem and had a flash size which was not a multiple of 4 bytes, too.
I can program the hex-file with ST-Link-Utility and debug with TrueStudio by removing the load-instruction from the startup file, but of course that's not convenient.
Solved! Go to Solution.
2018-10-31 2:15 PM
I had the same problem.
Update to the new Atollic version 9.1.0. This solved the question to me.
2018-08-09 9:27 PM
@AtollicSupport
2018-10-31 2:15 PM
I had the same problem.
Update to the new Atollic version 9.1.0. This solved the question to me.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.