2016-02-11 11:21 AM
Hello,
I am trying to flash my stm32429I-Eval via RS-232 using Flash Loader Demonstrator (v2.8).
I set SW1 & SW2 high (BOOT0/BOOT1), and reset the board. Run the demo GUI with default settings (baud=115.2k, Parity=Even, Echo=Off, Timeout=10). I get an �Unrecognized device� error.The config file does not have a definition for a STM32F4xx device.
[MCUs]
f1=STM32F1 f2=STR75x f3=STM8 f4=STR91xFA f5=STM32L1 f6=STM32F2 f7=STM32F0 f8=STM32L4I tried adding:
f9=STM32F4[f9]
ADDR_FLASH_SIZE=1FFF0000; START_FLASH_ADDR=08000000;I get the same result. What am I doing wrong?
#flash-loader-demo-stm32429i-evalWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.