2020-04-23 3:37 AM
Hello, I need to save data to the internal flash memory of my device. Naturally, I have opened the example that comes with the stm32cube for stm32g0 series. More specifically, I have compiled it for Nucelo-g070rb under System Workbench for stm32.
The example gets stuck on different places, depending on the optimization level. For no optimization, it jumps from HAL_FLASHEx_Erase to some invalid address and then halts.
For other optimization levels, it seemingly gets stuck on "BSP_LED_On(LED4);" (line 210), which should turn on when no error was detected during the process...
The debugger also runs into problems when this happens, stating the device was disconnected.
I have tried reducing the size of the erased memory to just a few pages and have also checked some of the addresses the example attempts to write to against the datasheet. It seems alright...
The code is the "FLASH_EraseProgram" example. I cannot append it due to size restrictions of this post. Here is the pastebin link. Thank you very much for your help!
2020-04-23 6:24 AM
Are you erasing flash pages in use by your program?
2020-04-23 7:35 AM
Aha! That was it! I have only tried to reduce the erased space, but it actually seems like the example is trying to erase the memory where the program is stored!
#define FLASH_USER_START_ADDR (FLASH_BASE + (20 * FLASH_PAGE_SIZE)) /* Start @ of user Flash area */
#define FLASH_USER_END_ADDR FLASH_BASE+(25*FLASH_PAGE_SIZE)-1//(FLASH_BASE + FLASH_SIZE - 1) /* End @ of user Flash area */
^-- this works! There is an error in the example... Thanks for your help!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.