2014-11-06 11:08 AM
Hi
we are using STM3220EVAL-G evaluation board.
In our project we want to establish two UARTs communication with two different external devices in Interrupt mode
UART related function are defined in
STSW-STM32062 (standard peripheral library)
How to relate STSW-STM32062 (standard peripheral library) with STM32CubeF2. because we need USB Host application also in our project. or shall we get UART examples implemented using HAL_UART functions available in
STM32CubeF2
(without DMA) in interrupt mode
Waiting for response Thanks
2014-11-13 1:28 AM
Hi,
Since you're using the STM32CubeF2 embedded software solution for USB Host application, it should be better that you use also the HAL UART driver to establish the communication between your STM32 and the external devices.The STM32CubeF2 package doesn't inclue any UART example in interrupt mode, you can refer to thehttp://www.st.com/web/catalog/tools/FM147/CL1794/SC961/SS1743/LN1897/PF259243
package under Projects\STM32F4-Discovery\ExamplesUART_TwoBoards_ComITNote that the STM32Cube HAL hardware abstraction layer, is enabling portability between different STM32 devices via standardized API calls.Regards,Heisenberg.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.