2024-02-28 8:18 AM
Hallo,
I'm using U5A9NJQ demoboard with FILEX. I have something that doesn't work, the first time I write on a file, all is correct, but if I rewrite on the same portion of the file, the writing seems to be correct, but, when reading, the content hasn't changed. Do you have found something similar? Is there a project where is possible to have the FILEX working with this demoboard?
Thank you
Solved! Go to Solution.
2024-09-06 1:26 AM
The problem was that when I was reading, I wasn't positioned in the correct position with fileseek.
2024-02-28 11:07 AM
Hello @IVent.1 ,
I advise you to follow this article which guides you on how to use FileX and contains the useful resources:
How to use FileX with eMMC for file system managem... - STMicroelectronics Community
2024-03-17 2:05 AM
2024-09-06 1:26 AM
The problem was that when I was reading, I wasn't positioned in the correct position with fileseek.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.