cancel
Showing results for 
Search instead for 
Did you mean: 

FIFO question ?

antonius
Senior

Dear Members,

How can I save FIFO ?

I have a psedo code :

for (i = 0; i < NUM_SAMPLES_TO_READ; i++) {

Read FIFO_DATA;

Save IR[15:8];

Read FIFO_DATA;

Save IR[7:0];

Read FIFO_DATA;

Save R[15:8];

Read FIFO_DATA;

Save R[7:0];

}

STOP;

my code :

   for(i=0;i<=number_sample;i++)

  {   

      printf("The output from MAX30100, from 0x09 register (FIFO DATA) : %u \r\n", buffer_rx[i]);

  } 

what should I add there ?

thanks

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
antonius
Senior

correct me ?

	  HAL_I2C_Master_Receive(&hi2c2, 0xAF, buffer_rx ,number_sample, 100); //receive 4 bytes from MAX30100
	for(i=0;i<=number_sample;i++)
   {	
		  FIFO_IR_samples[i]     =   buffer_rx[ ( i << 2 ) ];
      FIFO_IR_samples[i]   <<=   8U;
      FIFO_IR_samples[i]    |=   buffer_rx[ ( i << 2 ) + 1 ];
		 		 printf("Output MAX30100,0x09 register (FIFO DATA) IR : %u \r\n", FIFO_IR_samples[i]);
		   FIFO_RED_samples[i]     =   buffer_rx[ ( i << 2 ) ];
      FIFO_RED_samples[i]   <<=   8U;
      FIFO_RED_samples[i]    |=   buffer_rx[ ( i << 2 ) + 1 ];
		 
		 printf("Output MAX30100,0x09 register (FIFO DATA) RED : %u \r\n", FIFO_RED_samples[i]);
   }  

S.Ma
Principal

There are some code in git to dig in...

https://github.com/kontakt/MAX30100

https://www.arduinolibraries.info/libraries/max30100

 Obsolete item at Digikey...

uint8_t buffer_rx[32*4];
int32_t j;
#define MAKEWORD(b, a)	((uint16_t)(((uint8_t)(a)) | ((uint16_t)((uint8_t)(b))) << 8))
  HAL_I2C_Master_Receive(&hi2c2, 0xAF, buffer_rx ,number_sample*4, 100); //receive 4 bytes from MAX30100
for(i=j=0;i<=number_sample;i++,j+=4)
{	
  FIFO_IR_samples[i]     =  MAKEWORD( buffer_rx[ j+0 ],  buffer_rx[ j+1 ] );
  FIFO_RED_samples[i]     =  MAKEWORD( buffer_rx[ j+2 ], buffer_rx[ j+3 ] );
  printf("Output MAX30100,0x09 register (FIFO DATA) IR : %u , RED: %u \r\n", FIFO_IR_samples[i]), FIFO_RED_samples[i]);
}

antonius
Senior

Is my filter right ?

void filter(sample *s)
{
    uint8_t i;
    uint32_t red = 0;
    uint32_t ired = 0;
    for (i = 0; i < filter_level - 1; i++)
    {
        red += samplebuff[i].red;
        ired += samplebuff[i].ired;
    }
    s->red = (red + s->red) / filter_level;
    s->ired = (ired + s->ired) / filter_level;
}
 
void buffinsert(sample s)
{
    uint8_t i;
    for (i = buff_size - 1; i > 0; i--)
    {
        samplebuff[i].red = samplebuff[i - 1].red;
        samplebuff[i].ired = samplebuff[i - 1].ired;
    }
    samplebuff[0].red = s.red;
    samplebuff[0].ired = s.ired;
}
 
void calacdc(uint16_t *rac, uint32_t *rdc, uint16_t *iac, uint32_t *idc)
{
    uint32_t rmax = samplebuff[0].red;
    uint32_t rmin = samplebuff[0].red;
    uint32_t imax = samplebuff[0].ired;
    uint32_t imin = samplebuff[0].ired;
 
    uint8_t i;
    for (i = 0; i < buff_size; i++)
    {
        if (samplebuff[i].red > rmax)
            rmax = samplebuff[i].red;
        if (samplebuff[i].red < rmin)
            rmin = samplebuff[i].red;
        if (samplebuff[i].ired > imax)
            imax = samplebuff[i].ired;
        if (samplebuff[i].ired < imin)
            imin = samplebuff[i].ired;
    }
    *rac = rmax - rmin;
    *rdc = (rmax + rmin) / 2;
    *iac = imax - imin;
    *idc = (imax + imin) / 2;
}

Inside the loop :

	  HAL_I2C_Master_Receive(&hi2c2, 0xAF, buffer_rx ,number_sample*4, 100); //receive 4 bytes from MAX30100
	for(i=j=0;i<=number_sample;i++,j+=4)
   {	
		  samplebuff[i].ired    = buffer_rx[ j ];
		  samplebuff[i].ired   <<=   8U;
		  samplebuff[i].ired   |=   buffer_rx[ j + 1 ];
		  printf("Data %u ",i);
		  printf("Output MAX30100,0x09 register (FIFO DATA) IR : %u \r\n", samplebuff[i].ired);
		  //FIFO_IR_samples[i]     =   buffer_rx[ j ];
      //FIFO_IR_samples[i]   <<=   8U;
      //FIFO_IR_samples[i]    |=   buffer_rx[ j + 1 ];
		 		 //printf("Output MAX30100,0x09 register (FIFO DATA) IR : %u \r\n", FIFO_IR_samples[i]);
		 //Filter it
		 
		 //samplebufftemp[i].ired = FIFO_IR_samples[i];
		 samplebufftemp[i].ired = samplebuff[i].ired;
		 
		 buffinsert(samplebufftemp[i]);
		 calacdc(&redac, &reddc, &iredac, &ireddc);
		 filter(&samplebufftemp[i]);
		 
		 
		  //FIFO_RED_samples[i]     =   buffer_rx[ j+2 ];
      //FIFO_RED_samples[i]   <<=   8U;
      //FIFO_RED_samples[i]    |=   buffer_rx[  j+3 ];
		  samplebuff[i].red    = buffer_rx[ j ];
		  samplebuff[i].red   <<=   8U;
		  samplebuff[i].red   |=   buffer_rx[ j + 1 ];
		  printf("Data %u ",i);	
		 printf("Output MAX30100,0x09 register (FIFO DATA) RED : %u \r\n", samplebuff[i].red);
   
 	 //samplebufftemp[i].red = FIFO_RED_samples[i];
	  samplebufftemp[i].red = samplebuff[i].red;
		 buffinsert(samplebufftemp[i]); 
	   calacdc(&redac, &reddc, &iredac, &ireddc);
		 filter(&samplebufftemp[i]);
		 
		 float r = (((float)(redac)) / ((float)(reddc))) / (((float)(iredac)) / ((float)(ireddc)));
        if (r >= 0.36 && r < 0.66)
            spo2 = (uint8_t)(107 - 20 * r);
				    
        else if (r >= 0.66 && r < 1)
            spo2 = (uint8_t)(129.64 - 54 * r);
				     printf("SPO2 = %u\r\n",spo2);
				 static uint8_t eachbeatsamplecount = 0;    //????????????
         static uint8_t lasttenbeatsamplecount[10]; //?????????????
         static uint32_t last_ired = 0;  
         uint8_t ii;
				
				 eachsamplediff = last_ired - samplebufftemp[i].ired;
        if (eachsamplediff > 50 && eachbeatsamplecount > 12)
        {
            for (ii = 9; ii > 0; ii--)
                lasttenbeatsamplecount[i] = lasttenbeatsamplecount[i - 1];
            lasttenbeatsamplecount[0] = eachbeatsamplecount;
            uint32_t totaltime = 0;
            for (ii = 0; ii < 10; ii++)
                totaltime += lasttenbeatsamplecount[i];
            heartrate = (uint8_t)(60.0 * 10 / 0.02 / ((float)totaltime));
					    printf("Heart Rate = %u\r\n",heartrate);
            eachbeatsamplecount = 0;
        }
        last_ired = samplebufftemp[i].ired;
        eachbeatsamplecount++;
		 
 	 }  

global variable :

	 #define buff_size 50
		sample samplebuff[buff_size];
    sample samplebufftemp[buff_size];
		
		uint8_t heartrate = 0;
		uint8_t spo2 = 0;
 
		uint16_t redac = 0;
		uint32_t reddc = 0;
		uint16_t iredac = 0;
		uint32_t ireddc = 0;
		int16_t eachsamplediff = 0; 
 
#define filter_level 8 
   

antonius
Senior

I got the output :

Data 0 Output MAX30100,0x09 register (FIFO DATA) IR : 22337 
                  
Data 0 Output MAX30100,0x09 register (FIFO DATA) RED : 22337 
                 
SPO2 = 0
                                                                      
Data 1 Output MAX30100,0x09 register (FIFO DATA) IR : 30557 
                  
Data 1 Output MAX30100,0x09 register (FIFO DATA) RED : 30557 
                 
SPO2 = 0
                                                                      
Data 2 Output MAX30100,0x09 register (FIFO DATA) IR : 38668 
                  
Data 2 Output MAX30100,0x09 register (FIFO DATA) RED : 38668 
                 
SPO2 = 0
                                                                      
Data 3 Output MAX30100,0x09 register (FIFO DATA) IR : 46878 
                  
Data 3 Output MAX30100,0x09 register (FIFO DATA) RED : 46878 
                 
SPO2 = 0
                                                                      
Data 4 Output MAX30100,0x09 register (FIFO DATA) IR : 55170 
                  
Data 4 Output MAX30100,0x09 register (FIFO DATA) RED : 55170 
                 
SPO2 = 0
                                                                      
Data 5 Output MAX30100,0x09 register (FIFO DATA) IR : 63290 
                  
Data 5 Output MAX30100,0x09 register (FIFO DATA) RED : 63290 
                 
SPO2 = 0
                                                                      
Data 6 Output MAX30100,0x09 register (FIFO DATA) IR : 65535 
                  
Data 6 Output MAX30100,0x09 register (FIFO DATA) RED : 65535 
                 
SPO2 = 0
                                                                      
Data 7 Output MAX30100,0x09 register (FIFO DATA) IR : 65535 
                  
Data 7 Output MAX30100,0x09 register (FIFO DATA) RED : 65535 
                 
SPO2 = 0
                                                                      
Data 8 Output MAX30100,0x09 register (FIFO DATA) IR : 0 
                      
Data 8 Output MAX30100,0x09 register (FIFO DATA) RED : 0 
                     
SPO2 = 0
                                                      

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.