2018-07-25 12:17 AM
Hi there,
I'm using stm32F411 MCU
I configured the UART6 to transmit data with DMA.
Once in a while i'm getting FIFO ERROR from the DMA even though i'm using direct mode and not FIFO mode.
Although the error occur, the data is still transfer successfully.
what can cause this error?
thanks.
2018-08-01 4:56 PM
I checked your chip, this is not trivial.
mode 1 or mode 2 ?
surely you can find an example of the schematic
2018-08-07 3:56 AM
this is the configuration of the DMA i use for RX:
hdma_rx.Init.Direction = DMA_PERIPH_TO_MEMPRY;
hdma_rx.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_rx.Init.MemInc = DMA_MINC_ENABLE;
hdma_rx.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;
hdma_rx.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;
hdma_rx.Init.Mode = DMA_CIRCULAR;
hdma_rx.Init.Priority = DMA_PRIORITY_LOW;
hdma_rx.Init.FIFOMode = DMA_FIFOMODE_DISABLE;
Other than that, i'm using STM32 standard HAL driver for receiving from uart.
the HAL driver version is 1.18
thanks
2018-08-07 5:36 AM
For explanation, see AN4031, chapter 4.3 Software sequence to enable DMA.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.