2018-08-25 3:33 PM
Hello, I´m working with the STM32Cube_FW_F4_V1.21.0 and the STM32F446E_EVAL and the LibJPEG example in the Application file, with the 32f446VE in a board made by my self, the cubeMx version is the 4.21.0, and everything works even the JPEG compression, the problem is when I use the FATFS_LinkDriver() function, becouse after executed and entering to the f_mount() function the program fails, otherwise whent I comment FATFS_LinkDriver(), the program works normal, the FAT functions works and compress the immage inside de SD Card and save the new JPEG image.
Any advise or suggestion to fix this problem please, cause I want to add more drivers like SD memory and USB, and I don`t want to have problems with this in future.
Regards
2018-08-25 4:30 PM
Fails how? What error?
You're going to have do dig a bit, all the source is available to debug through. Step through f_mount() to see what it's issue is, and then work backward.
Look specifically at the disk structure, and that is is big enough, check _VOLUMES define. Check the path parameter describes at least 4 bytes.
2018-08-26 8:45 AM
Hi Clive Two.Zero, When I use FATFS_LinkDriver(), the next functioin, f_mount() hangs completely, and if I debbug to get into this my IDE(IAR) became blocked. Here is my code in main, as I said, It is jus a copy paste from the examples.
Thanks
/* Includes ------------------------------------------------------------------*/
#include "main.h"
#include "stm32f4xx_hal.h"
#include "fatfs.h"
/* USER CODE BEGIN Includes */
/* USER CODE END Includes */
/* Private variables ---------------------------------------------------------*/
SD_HandleTypeDef hsd;
/* USER CODE BEGIN PV */
/* Private variables ---------------------------------------------------------*/
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_SDIO_SD_Init(void);
/* USER CODE BEGIN PFP */
/* Private function prototypes -----------------------------------------------*/
/* USER CODE END PFP */
/* USER CODE BEGIN 0 */
FATFS myFatFS;
FIL myFile;
UINT myBytes;
/* USER CODE END 0 */
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration----------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_SDIO_SD_Init();
MX_FATFS_Init();
/* USER CODE BEGIN 2 */
/*##-2- Link the micro SD disk I/O driver ##################################*/
if(FATFS_LinkDriver(&SD_Driver, SD_Path) == 0)
{
if(f_mount(&myFatFS, SD_Path, 0) ==FR_OK)
{
char myFileName[] = "TEST1.txt";
if(f_open(&myFile, myFileName, FA_WRITE | FA_CREATE_ALWAYS) == FR_OK)
{
char myData[] = "Hello from fuckyou";
if(f_write(&myFile, myData, sizeof(myData), &myBytes) == FR_OK)
{
__NOP();
}
f_close(&myFile);
}
}
}
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
/** System Clock Configuration
*/
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct;
RCC_ClkInitTypeDef RCC_ClkInitStruct;
RCC_PeriphCLKInitTypeDef PeriphClkInitStruct;
/**Configure the main internal regulator output voltage
*/
__HAL_RCC_PWR_CLK_ENABLE();
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
/**Initializes the CPU, AHB and APB busses clocks
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_ON;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL.PLLM = 6;
RCC_OscInitStruct.PLL.PLLN = 180;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
RCC_OscInitStruct.PLL.PLLQ = 8;
RCC_OscInitStruct.PLL.PLLR = 2;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
/**Activate the Over-Drive mode
*/
if (HAL_PWREx_EnableOverDrive() != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
/**Initializes the CPU, AHB and APB busses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_SDIO|RCC_PERIPHCLK_CLK48;
PeriphClkInitStruct.Clk48ClockSelection = RCC_CLK48CLKSOURCE_PLLQ;
PeriphClkInitStruct.SdioClockSelection = RCC_SDIOCLKSOURCE_CLK48;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
/**Configure the Systick interrupt time
*/
HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000);
/**Configure the Systick
*/
HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK);
/* SysTick_IRQn interrupt configuration */
HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0);
}
/* SDIO init function */
static void MX_SDIO_SD_Init(void)
{
hsd.Instance = SDIO;
hsd.Init.ClockEdge = SDIO_CLOCK_EDGE_RISING;
hsd.Init.ClockBypass = SDIO_CLOCK_BYPASS_DISABLE;
hsd.Init.ClockPowerSave = SDIO_CLOCK_POWER_SAVE_DISABLE;
hsd.Init.BusWide = SDIO_BUS_WIDE_1B;
hsd.Init.HardwareFlowControl = SDIO_HARDWARE_FLOW_CONTROL_DISABLE;
hsd.Init.ClockDiv = 3;
}
/** Configure pins as
* Analog
* Input
* Output
* EVENT_OUT
* EXTI
*/
static void MX_GPIO_Init(void)
{
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOH_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE();
__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_RCC_GPIOD_CLK_ENABLE();
}
/* USER CODE BEGIN 4 */
/* USER CODE END 4 */
/**
* @brief This function is executed in case of error occurrence.
* @param None
* @retval None
*/
void _Error_Handler(char * file, int line)
{
/* USER CODE BEGIN Error_Handler_Debug */
/* User can add his own implementation to report the HAL error return state */
while(1)
{
}
/* USER CODE END Error_Handler_Debug */
}
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @param file: pointer to the source file name
* @param line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t* file, uint32_t line)
{
/* USER CODE BEGIN 6 */
/* User can add his own implementation to report the file name and line number,
ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
/* USER CODE END 6 */
}
#endif
2018-08-26 9:04 AM
This is top level code, you need to dig deeper to understand why/where IAR is blocking. Stop the execution and see where it is (hardfault or default handler). Make sure you have the IRQ handlers for the SDIO, and you have a Hard Fault Handler that outputs useful diagnostic information rather than spin in while(1) loop.
char SDPath[4]; /* SD card logical drive path */
2018-08-27 5:54 PM
Hi Clive Two.Zero, the problem is fixed, in the initialation MX_FATFS_Init(), is already declared the function FATFS_LinkDriver, so I was using the funtion twice and that might be causing the error.
Thanks for your help.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.