2016-01-04 5:42 PM
Hello all,
I am new around here; please excuse in advance my probably boring query... I have a custom board with an STM32F427ZI together with 256Mb of SDRAM (the chip is an AS4C16M16S). I configured it with the code below (not understanding fully what I am doing). My problem is that I can access only the first 128KB after address 0xD0000000. If I go past this point it HardFaults, (or read only zeroes depending on the particular configurations I tried). Could a good soul take a look at the code, and/or hint at a direction where to go?<pre> FMCT.FMC_LoadToActiveDelay = 2; // 2 1 clock cycle = 1 / 90MHz = 11ns FMCT.FMC_ExitSelfRefreshDelay = 6; // 6 TXSR: min=66ns ( 6x11ns) FMCT.FMC_SelfRefreshTime = 4; // 4 TRAS: min=44ns ( 4x11ns) max = 120k (ns) FMCT.FMC_RowCycleDelay = 6; // 6 TRC: min=66ns ( 7x11ns) FMCT.FMC_WriteRecoveryTime = 2; // 2 TWR: min=1+7ns (1+1x11ns) FMCT.FMC_RPDelay = 2; // 2 TRP: 20ns ( 2x11ns) FMCT.FMC_RCDDelay = 2; // 2 TRCD: 20ns ( 2x11ns) FMCI.FMC_Bank = FMC_Bank2_SDRAM; // FMC SDRAM control configuration FMCI.FMC_ColumnBitsNumber = FMC_ColumnBits_Number_9b; // Row addressing : [ 8:0] FMCI.FMC_RowBitsNumber = FMC_RowBits_Number_12b; // Column addressing: [11:0] FMCI.FMC_SDMemoryDataWidth = FMC_SDMemory_Width_16b; FMCI.FMC_InternalBankNumber = FMC_InternalBank_Number_4; FMCI.FMC_CASLatency = FMC_CAS_Latency_3; // CL: Cas Latency = 3 clock cycles FMCI.FMC_WriteProtection = FMC_Write_Protection_Disable; FMCI.FMC_SDClockPeriod = FMC_SDClock_Period_2; FMCI.FMC_ReadBurst = FMC_Read_Burst_Disable; FMCI.FMC_ReadPipeDelay = FMC_ReadPipe_Delay_1; FMCI.FMC_SDRAMTimingStruct = &FMCT; FMC_SDRAMInit(&FMCI); // FMC SDRAM bank initialization // Configure a clock configuration enable command FMCC.FMC_CommandMode = FMC_Command_Mode_CLK_Enabled; FMCC.FMC_CommandTarget = FMC_Command_Target_bank2; FMCC.FMC_AutoRefreshNumber = 1; FMCC.FMC_ModeRegisterDefinition = 0; while(FMC_GetFlagStatus(FMC_Bank2_SDRAM, FMC_FLAG_Busy) != RESET); FMC_SDRAMCmdConfig(&FMCC); for(timeout = 0x00; timeout < 0xD0000; timeout++) {} // Configure a PALL (precharge all) command FMCC.FMC_CommandMode = FMC_Command_Mode_PALL; FMCC.FMC_CommandTarget = FMC_Command_Target_bank2; FMCC.FMC_AutoRefreshNumber = 1; FMCC.FMC_ModeRegisterDefinition = 0; while(FMC_GetFlagStatus(FMC_Bank2_SDRAM, FMC_FLAG_Busy)); FMC_SDRAMCmdConfig(&FMCC); // Configure a Auto-Refresh command FMCC.FMC_CommandMode = FMC_Command_Mode_AutoRefresh; FMCC.FMC_CommandTarget = FMC_Command_Target_bank2; FMCC.FMC_AutoRefreshNumber = 1; FMCC.FMC_ModeRegisterDefinition = 0; while(FMC_GetFlagStatus(FMC_Bank2_SDRAM, FMC_FLAG_Busy)); FMC_SDRAMCmdConfig(&FMCC); // Configure a load Mode register command&sharpdefine SDRAM_BURST_LENGTH_1 ((uint16_t)0x0000)&sharpdefine SDRAM_BURST_LENGTH_2 ((uint16_t)0x0001)&sharpdefine SDRAM_BURST_LENGTH_4 ((uint16_t)0x0002)&sharpdefine SDRAM_BURST_LENGTH_8 ((uint16_t)0x0004)&sharpdefine SDRAM_BURST_TYPE_SEQUENTIAL ((uint16_t)0x0000)&sharpdefine SDRAM_BURST_TYPE_INTERLEAVED ((uint16_t)0x0008)&sharpdefine SDRAM_CAS_LATENCY_2 ((uint16_t)0x0020)&sharpdefine SDRAM_CAS_LATENCY_3 ((uint16_t)0x0030)&sharpdefine SDRAM_OPERATING_MODE_STANDARD ((uint16_t)0x0000)&sharpdefine SDRAM_WRITEBURST_MODE_PROGRAMMED ((uint16_t)0x0000)&sharpdefine SDRAM_WRITEBURST_MODE_SINGLE ((uint16_t)0x0200)&sharpdefine SDRAM_MODEREG (SDRAM_BURST_LENGTH_2|SDRAM_BURST_TYPE_SEQUENTIAL|SDRAM_CAS_LATENCY_3|SDRAM_OPERATING_MODE_STANDARD|SDRAM_WRITEBURST_MODE_SINGLE) FMCC.FMC_CommandMode = FMC_Command_Mode_LoadMode; FMCC.FMC_CommandTarget = FMC_Command_Target_bank2; FMCC.FMC_AutoRefreshNumber = 1; FMCC.FMC_ModeRegisterDefinition = SDRAM_MODEREG; while(FMC_GetFlagStatus(FMC_Bank2_SDRAM, FMC_FLAG_Busy)); FMC_SDRAMCmdConfig(&FMCC); // Set the refresh rate counter // (15.6 us x Freq) - 20 = (15.6 * 90MHz) - 20 = 1384 // Set the device refresh counter FMC_SetRefreshCount(1384); while(FMC_GetFlagStatus(FMC_Bank2_SDRAM, FMC_FLAG_Busy) != RESET);</pre>
#sdram2016-01-04 6:36 PM
Please show the code that Hard Faults
2016-01-05 3:41 AM
Hello clive1, thanks for helping. I've read many of your post which were very helpful.
False alarm... I had spent so much time debugging SDRAM issue that it didn't occur to me that the problem could have come from somewhere else (which your message suggested). It now works perfectly fine!Sorry about this.2016-01-05 5:04 AM
which your message suggested
Glad you caught that. No need to be sorry.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.