STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

HAL USB odd/even issue for OUT endpoints

Posted on January 05, 2016 at 13:49When preparing to receive the data on OUT isochronous endpoint, the HAL sets up the even/odd flag once when you call the PrepareReceive for that specific frame that is active at that moment.However the data may com...

STM32F103 Flash Erase Error

Posted on January 02, 2016 at 10:53My Flash is divided into 3 parts first part of code only decide that which part is active b/w the remaining two parts and jumps to the active part accordingly. The remaining inactive part is for remote firmware upd...

STMStudio Issues

Posted on January 04, 2016 at 10:43Good morning,recently my company has renewed its workstation park with some machines running windows 7 pro 64 bits. The issue is that since this upgrade we're no longer able to use STMStudio efficiently: data visua...

labprog by Associate
  • 1782 Views
  • 1 replies
  • 0 kudos

TIM INTERRUPT IRQ STM32F3DISCOVERY

Posted on January 04, 2016 at 16:17 Hi all, I'd like to have e PWM signal, starting with a duty cycle of 10% and incrementing up to 100%. I'm using next code, I see the waveform with 10%, but it never increase, it seems that it never enter ...

USB OTG OUT packet receiving problem

Posted on January 05, 2016 at 08:28In HAL STM32F4xx_LL_USB_DRIVER in function USB_EPStartXfer for isochronous OUT endpoint the odd/even flag is always setup to the inverse of current odd/even frame.I wonder if that is the problem when receiving the ...

USB OTG OUT packet receiving problem

Posted on January 05, 2016 at 08:22In HAL STM32F4xx_LL_USB_DRIVER in function USB_EPStartXfer for isochronous OUT endpoint the odd/even flag is always setup to the inverse of current odd/even frame.I wonder if that is the problem when receiving the ...

STM32F401RE Timer setup

Posted on December 24, 2015 at 18:32Hi, I'm getting started with the 'F401 device, I'm trying to blink the LED on the Nucleo-F401RE board when Timer2 triggers. I know this is just register level stuff and I'm probably making things harder for myself...

stforum by Associate II
  • 3586 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.