2017-07-26 2:15 AM
Hi,
After the jumping bootloader, the EXTI_line7 not work!boot.c
/* Test if user code is programmed starting from address 'APPLICATION_ADDRESS' */
if (((*(__IO uint32_t*)FLASH_USER_START_ADDR) & 0x2FFE0000 ) == 0x20000000) { /* Jump to user application */ JumpAddress = *(__IO uint32_t*) (FLASH_USER_START_ADDR + 4); Jump_To_Application = (pFunction) JumpAddress; /* Initialize user application's Stack Pointer */ __set_MSP(*(__IO uint32_t*) FLASH_USER_START_ADDR); __disable_irq(); /* Jump to application */ Jump_To_Application(); }application.cint main(void)
{ unsigned long ulChk = 0; unsigned int uiLen = 0; GPIO_InitTypeDef GPIO_InitStructure; uint32_t i = 0;RCC_APB2PeriphClockCmd(RCC_APB2Periph_SYSCFG, ENABLE); // Clock not Reset
/* Relocate by software the vector table to the internal SRAM at 0x20000000 ***/
/* Copy the vector table from the Flash (mapped at the base of the application load address 0x08003000) to the base address of the SRAM at 0x20000000. */ for(i = 0; i < 48; i++) { VectorTable[i] = *(__IO uint32_t*)(APPLICATION_ADDRESS + (i<<2)); }/* Enable the SYSCFG peripheral clock*/
RCC_APB2PeriphResetCmd(RCC_APB2Periph_SYSCFG, ENABLE); /* Remap SRAM at 0x00000000 */ SYSCFG_MemoryRemapConfig(SYSCFG_MemoryRemap_SRAM);/***************** Add your application code here ***************************/
/* Unlock the Flash Program Erase controller */
FLASH_Unlock();// main loop...
}
I'm have add SYSCFG clock enabled prior to remapping the RAM, but EXTI line 7 not work!
thanks
Solved! Go to Solution.
2017-11-17 1:01 AM
I have solved!
it is necessary used the EXTI pin on port A. If bootloader and application is used, the EXTI pin only works if it is on port A.
It is necessary that EXTI pin is configured in boot code and in application code.
good job!
2017-08-24 11:58 PM
The exti line 7 is working if not used bootloather.
If loaded the same application code with bootloather the exti line 7 not working.
Suggestions
?
2017-11-17 1:01 AM
I have solved!
it is necessary used the EXTI pin on port A. If bootloader and application is used, the EXTI pin only works if it is on port A.
It is necessary that EXTI pin is configured in boot code and in application code.
good job!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.