2017-04-18 11:28 AM
AN4621 'STM32L4 ultra-low-power features overview' says (page 16):
The STM32L4A6xG, thanks to the external SMPS supply option, makes it possible to force on the Vcore pins (when the MR is in use) an external VDD12 supply. When VDD12 is forced by an external source and is higher than the output of the internal LDO, the current is taken from this external supply and the overall power efficiency is significantly improved when using an external step down DC/DC converter.
I just checked the STM32L4A6xG datasheet, and none of the packages show a VDD12 pin. So, simple question I guess: What happened to external SMPS support? Was it cut from the product?
2017-04-18 2:37 PM
The STM32L496xx datasheet know about a P option. Look on page 75 and '8 Part numbering'. However distributor availabilty is not (yet?) given.
2017-04-18 4:50 PM
Fascinating. So the STM32L4A6xx datasheet does not have this (the P option in the part-numbering table), even though AN4621 claims that the VDD12 pin is *only* available on the STM32L4A6 devices, and not on any others! It would appear that app note is just plain wrong, because I discovered a more recent app note, AN4978, which lists the applicable products as
STM32L452RE, STM32L476ZG, STM32L496RG, STM32L496AG, STM32L496ZG, STM32L496VE, STM32L433RC
Sigh. ST, would you please prioritize your documentation? And get some people who can write, while you're at it...
2017-04-19 2:42 AM
Hi
Haun.Mark
,We confirm the issue related to the
AN4621 and it will be fixed in coming release of the document.
Thank you for bringing this issue to our attention and Sorry for the inconvenience it may bring.
-Nesrine-
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.