2017-11-17 2:06 PM
Hello,
I am trying to find examples of code where the external SRAM is mapped using the linker file. I saw an example of it being done here (
https://community.st.com/0D50X00009XkfB3SAJ
). However, all the uses of the SRAM eg.[the HAL_SRAM_Write_32b() function] in the example code make use of locking. If anyone has examples of using external RAM as general purpose RAM it would be greatly appreciated.FYI this is being done on the STM32L496G-DISCO board
null2017-11-24 6:24 AM
Hello Chris, did you able to success with external SRAM access?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.