2012-01-03 5:44 AM
Hello
I have to try use an external memory for writing and reading same data on stm32 discovery board.Which type memory can i use ? EEPROM or FLASH ? And how can i connect this device to my board ?Is there anyone tried about it #stm32 #memory #gpio2012-01-03 7:44 AM
Hi.
You can use EEPROM or Flash as you prefer, the main difference between the two technologies are access time (EEPROM is slower) and life span (longer for EEPROM). Also on my opinion EEPROM is simpler to use because you can erase one byte a time but if you need quick read/write cycles or lot of memory, Flash would be a better choice. To connect your memory on your board you can use I2C (look at the STM32C-Eval board schematics, it uses an EEPROM linked to the micro with I2C, and an example how to use it is given in the standard library). SPI and parallel memories are also available (with SPI you can get higher transfer rates). Also if you don't really need an external memory the application note AN2594 explain how to use STM's internal Flash to emulate an EEPROM. And if you use the STM32L-Discovery the embedded micro have a ''true'' internal EEPROM. Hope it will help you. Regards. robin.2012-01-03 8:51 AM
hello Robin ,
the PDF mention an example application but I couldnot find it attached where can I download it ?2012-01-03 1:02 PM
2012-01-04 2:58 AM
Hi.
You have to download the STM32F10x Standard peripheral library. Follow the link : http://www.st.com/internet/mcu/product/221020.jsp then click on ''Design support'' and you'll find the library in the bottom of the page, paragraph ''Firmware''. In the library file the exemple is in ''Project\STM32F10x_StdPeriph_Examples\I2C\EEPROM'' Regards.2012-01-04 6:57 AM
2012-01-05 12:25 AM
I will try it ! thanks Robin
2012-01-05 12:27 AM
I will try it ! But my data is 3 or 4 mb so i want to make this way, however i will try again to emulate EEPROM to Flash Memory . thanks Robin
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.