2016-07-26 2:07 PM
I am trying to configure an external audio codec to work with the STM32F4 discovery board. I have got the onboard codec working via the spi driver (stm32f4xx_spi.c) and was wondering how I would have to configure things differently so that the data would be sent to the external codec instead. As is it seems like I could connect my external codec to the necessary GPIO pins, but the internal codec would be connected to these as well which would cause problems. Is it a matter of simply changing the GPIO pins, or would there be something more?
I use the following 2 methods to initialize codec control in my program:void codec_init(){ GPIO_InitTypeDef PinInitStruct; GPIO_StructInit(&PinInitStruct); I2S_InitTypeDef I2S_InitType; I2C_InitTypeDef I2C_InitType; //Reset pin as GPIO PinInitStruct.GPIO_Pin = CODEC_RESET_PIN; PinInitStruct.GPIO_Mode = GPIO_Mode_OUT; PinInitStruct.GPIO_PuPd = GPIO_PuPd_DOWN; PinInitStruct.GPIO_OType = GPIO_OType_PP; PinInitStruct.GPIO_Speed = GPIO_Speed_50MHz; RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA | RCC_AHB1Periph_GPIOD | RCC_AHB1Periph_GPIOB, ENABLE); GPIO_Init(GPIOD, &PinInitStruct); // I2C pins PinInitStruct.GPIO_Mode = GPIO_Mode_AF; PinInitStruct.GPIO_OType = GPIO_OType_OD; PinInitStruct.GPIO_Pin = I2C_SCL_PIN | I2C_SDA_PIN; PinInitStruct.GPIO_PuPd = GPIO_PuPd_NOPULL; PinInitStruct.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOB, &PinInitStruct); GPIO_PinAFConfig(GPIOB, GPIO_PinSource6, GPIO_AF_I2C1); GPIO_PinAFConfig(GPIOB, GPIO_PinSource9, GPIO_AF_I2C1); //enable I2S and I2C clocks //RCC_I2SCLKConfig(RCC_I2S2CLKSource_PLLI2S); RCC_APB1PeriphClockCmd(RCC_APB1Periph_I2C1 | RCC_APB1Periph_SPI3, ENABLE); RCC_PLLI2SCmd(ENABLE); // I2S pins PinInitStruct.GPIO_OType = GPIO_OType_PP; PinInitStruct.GPIO_Pin = I2S3_SCLK_PIN | I2S3_SD_PIN | I2S3_MCLK_PIN; GPIO_Init(GPIOC, &PinInitStruct); PinInitStruct.GPIO_Pin = I2S3_WS_PIN; GPIO_Init(GPIOA, &PinInitStruct); //prepare output ports for alternate function GPIO_PinAFConfig(GPIOA, GPIO_PinSource4, GPIO_AF_SPI3); GPIO_PinAFConfig(GPIOC, GPIO_PinSource7, GPIO_AF_SPI3); GPIO_PinAFConfig(GPIOC, GPIO_PinSource10, GPIO_AF_SPI3); GPIO_PinAFConfig(GPIOC, GPIO_PinSource12, GPIO_AF_SPI3); //keep Codec off for now GPIO_ResetBits(GPIOD, CODEC_RESET_PIN); // configure I2S port SPI_I2S_DeInit(CODEC_I2S); I2S_InitType.I2S_AudioFreq = I2S_AudioFreq_48k; I2S_InitType.I2S_MCLKOutput = I2S_MCLKOutput_Enable; I2S_InitType.I2S_DataFormat = I2S_DataFormat_16b; I2S_InitType.I2S_Mode = I2S_Mode_MasterTx; I2S_InitType.I2S_Standard = I2S_Standard_Phillips; I2S_InitType.I2S_CPOL = I2S_CPOL_Low; I2S_Init(CODEC_I2S, &I2S_InitType); //I2S_Cmd(CODEC_I2S, ENABLE); // configure I2C port I2C_DeInit(CODEC_I2C); I2C_InitType.I2C_ClockSpeed = 100000; I2C_InitType.I2C_Mode = I2C_Mode_I2C; I2C_InitType.I2C_OwnAddress1 = CORE_I2C_ADDRESS; I2C_InitType.I2C_Ack = I2C_Ack_Enable; I2C_InitType.I2C_AcknowledgedAddress = I2C_AcknowledgedAddress_7bit; I2C_InitType.I2C_DutyCycle = I2C_DutyCycle_2; I2C_Cmd(CODEC_I2C, ENABLE); I2C_Init(CODEC_I2C, &I2C_InitType);}void codec_ctrl_init(){ uint32_t delaycount; uint8_t CodecCommandBuffer[5]; uint8_t regValue = 0xFF; GPIO_SetBits(GPIOD, CODEC_RESET_PIN); delaycount = 1000000; while (delaycount > 0) { delaycount--; } //keep codec OFF CodecCommandBuffer[0] = CODEC_MAP_PLAYBACK_CTRL1; CodecCommandBuffer[1] = 0x01; send_codec_ctrl(CodecCommandBuffer, 2); //begin initialization sequence (p. 32) CodecCommandBuffer[0] = 0x00; CodecCommandBuffer[1] = 0x99; send_codec_ctrl(CodecCommandBuffer, 2); CodecCommandBuffer[0] = 0x47; CodecCommandBuffer[1] = 0x80; send_codec_ctrl(CodecCommandBuffer, 2); regValue = read_codec_register(0x32); CodecCommandBuffer[0] = 0x32; CodecCommandBuffer[1] = regValue | 0x80; send_codec_ctrl(CodecCommandBuffer, 2); regValue = read_codec_register(0x32); CodecCommandBuffer[0] = 0x32; CodecCommandBuffer[1] = regValue & (~0x80); send_codec_ctrl(CodecCommandBuffer, 2); CodecCommandBuffer[0] = 0x00; CodecCommandBuffer[1] = 0x00; send_codec_ctrl(CodecCommandBuffer, 2); //end of initialization sequence CodecCommandBuffer[0] = CODEC_MAP_PWR_CTRL2; CodecCommandBuffer[1] = 0xAF; send_codec_ctrl(CodecCommandBuffer, 2); CodecCommandBuffer[0] = CODEC_MAP_PLAYBACK_CTRL1; CodecCommandBuffer[1] = 0x70; send_codec_ctrl(CodecCommandBuffer, 2); CodecCommandBuffer[0] = CODEC_MAP_CLK_CTRL; CodecCommandBuffer[1] = 0x81; //auto detect clock send_codec_ctrl(CodecCommandBuffer, 2); CodecCommandBuffer[0] = CODEC_MAP_IF_CTRL1; CodecCommandBuffer[1] = 0x07; send_codec_ctrl(CodecCommandBuffer, 2); CodecCommandBuffer[0] = 0x0A; CodecCommandBuffer[1] = 0x00; send_codec_ctrl(CodecCommandBuffer, 2); CodecCommandBuffer[0] = 0x27; CodecCommandBuffer[1] = 0x00; send_codec_ctrl(CodecCommandBuffer, 2); CodecCommandBuffer[0] = 0x1A | CODEC_MAPBYTE_INC; CodecCommandBuffer[1] = 0x0A; CodecCommandBuffer[2] = 0x0A; send_codec_ctrl(CodecCommandBuffer, 3); CodecCommandBuffer[0] = 0x1F; CodecCommandBuffer[1] = 0x0F; send_codec_ctrl(CodecCommandBuffer, 2); CodecCommandBuffer[0] = CODEC_MAP_PWR_CTRL1; CodecCommandBuffer[1] = 0x9E; send_codec_ctrl(CodecCommandBuffer, 2);} #i2s #codec-audio #external #!stm32f4-discoWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.