2016-07-26 8:28 AM
I have been using a busy for loop to create my delays, but now I need precision. I want a function that will wait for n microseconds. How should I go about doing this? The Systick timer is not accurate enough (already tried it).
2016-07-26 9:05 AM
DWT_CYCCNT you can count off CPU cycles, I've posted examples to the forum.
2016-07-26 11:23 AM
Thank you for pointing me in the right direction!
void
enable_delay(void){
DWT->CYCCNT = 0;
CoreDebug->DEMCR |= 0x01000000;
DWT->CTRL |= 1;
}
void
delay(uint32_t tick){
uint32_t start = DWT->CYCCNT;
uint32_t current = 0;
do{
current = DWT->CYCCNT;
}while((current - start) < tick);
}
2016-07-26 12:23 PM
@Community member: Why do you think that Systick is not accurate enough?
@Clive: Is it allowed to use DWT counter as a regular timer? Does it run with SYSCLK frequency? Is debugging not disturbed by using DWT?Thanks2016-07-26 12:49 PM
I could only get microsecond accuracy with
SysTick_Config(HAL_RCC_GetHCLKFreq()/1000000);
HAL_GetTick(); And yes it uses the SYSCLK. I was using the default on board clock speed 168 MHz. I don't know how it affects debugging.
2016-07-26 1:35 PM
SysTick typically clocks at 1/8th CPU speed, is only 24-bit, counts down, usually non-maximal, ... so it sucks the math up.
The DWT unit is on the silicon, you can use it or not, I've not had problems debugging. Clocks at CPU speed, is 32-bit, and counts up, @ 72MHz takes a minute to wrap, is thread/interrupt safe for delay loops. I'd define it as a free running counter rather than a timer, no provision for interrupt.Fastest 32-bit TIM run half clock speed (typically, on APB1)2016-07-26 2:16 PM
John, I asked about Systick accuracy because I thought that you don't know that it can run with SYSCLK too. You just have to configure that in its CONTROL register and then read its CURRENT register. At 72 MHz it takes approximately 233 ms to wrap around, if RELOAD register is set to full 24-bit.
Thanks Clive for clarification.2016-07-26 2:30 PM
The math on it is unduly burdensome, effectively diminishing the granularity, and most people use it for a 1ms / 1 KHz ticker.
An atomic 32-bit counter, pretty hard to fault..We’re moving the ST Community to a new platform to give you a better and more reliable community experience.