2022-11-21 4:17 AM
Hi there,
I am looking at STM32G031Kxxx (32pin LQFP) and am wondering whether it is possible to provide an external high speed clock source to this µC?
The datasheet shows that in this package OSC32_IN and OUT are available, but for the HSE, there is only OSC_IN.
So, a crystal cannot be used, but an external clock should be possible - if needed.
Is my assumption right?
Solved! Go to Solution.
2022-11-21 4:32 AM
I neglected to point out that only either OSC_IN or OSC32 is available in the 32pin package. Both at the same time are not possible with this package.
Regards
/Peter
2022-11-21 4:25 AM
Yes, your assumption is correct.
Regards
/Peter
2022-11-21 4:29 AM
Thanks!
2022-11-21 4:32 AM
I neglected to point out that only either OSC_IN or OSC32 is available in the 32pin package. Both at the same time are not possible with this package.
Regards
/Peter
2022-11-21 4:35 AM
yes, thank you
2022-11-21 4:36 AM
You're welcome!
If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.