2023-07-17 7:48 AM
Hi,
Would someone have a external ADC that works with SPI TI mode to recommend?
Thank you.
2023-07-18 4:47 AM
Hello @SebB,
The SPI interface is compatible with the TI protocol. (which is the default case)
However, I inform you that STM32F4 has his own internal ADCs. In fact, you must know, the 12-bit ADC is a successive approximation analog-to-digital converter. It has up to 19 multiplexed channels allowing it to measure signals from 16 external sources, two internal sources, and the VBAT channel. The A/D conversion of the channels can be performed in single, continuous, scan or discontinuous mode. The result of the ADC is stored into a left- or right-aligned 16-bit data register.
Would someone have a external ADC that works with SPI TI mode to recommend?
You must choose your ADC regarding your application and what you are searching in terms of :
- Resolution (bits)
- Architecture (Delta-Sigma, SAR...)
- Number of input channels
- SNR
- Price...
Best Regards,
Pierre
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.