2023-07-17 8:06 AM
Hello,
I have an STM32L4R9ZI controller connected to a computer running Windows 10. I have a custom protocol where the computer sends a command and my controller responds. I am using VCP to achieve this. The communication is established and operational. For some tests I require to send out commands and get responses continuously for days. The typical rate of communication is 5 commands a second. Every command contains a maximum 20 bytes and a response may contain up to 50 bytes.
While testing I have been facing issues when a response is not received by the PC and my test scripts fail. I have been trying to find out on forums about solving this problem and few articles point me towards a windows 10 driver issue in particular.
However, I am not sure whether:
1. It is the controller that does not receive the command to respond (PC did not send it) - This may not be the problem as some of the commands suggest that internal memory of my controller is written as a result of the command and hence it was sent out by the PC.
2. Controller did not respond - Would this be a problem that the controller sometimes does not respond? I use the CDC_Transmit_FS function to send out data.
3. Controller responded but PC did not receive it. It is python scripts that read my data out. I see the script timing out on the serial read.
This problem is very random. Sometimes I have seen it happen several times a day and sometimes my tests for 5 days have completed successfully. It happens on different commands so I am not attributing it to a single command being incorrectly coded.
Request for help with regards to how to solve / debug this please. I was thinking about using if there are any USB analyzers / sniffers.
I thank you in advance!
Makarand
2023-07-17 11:27 AM - edited 2023-07-17 11:31 AM
> few articles point me towards a windows 10 driver issue
Win10 driver issue? Any link or reference, please?
> I was thinking about using if there are any USB analyzers / sniffers.
A good idea. With a quality logging tool and automation. This already comes close to a professional-grade testing harness.
Arrange your commands and responses to be more helpful (add, for example, sequence numbers or other means to help detecting anomalies).
2023-07-18 1:26 AM
Hello,
Here are links that I was referring to indicating towards a Windows 10 driver problem.
One of the posts is also very old - around 2015.
> A good idea. With a quality logging tool and automation. This already comes close to a professional-grade testing harness. - Any ones you can recommend please?
Thanks,
Makarand
2023-07-18 1:43 AM
Thank you for the collection of references. I remember the last one, on the MSDN forum. Since no convincing repro had been provided (and the Windows dept. used to do a good QA then) these few reports were caused by bugs in device firmware for STM32 or other popular MCUs. It's unlikely a genuine bug in Windows usbser or USB core.
As for USB analyzer.... I have a very aged Ellisys. Hesitate to recommend it. Try "Hardware recommendations" on Stack overflow.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.