2017-06-22 7:46 AM
Hi guy's,
I'm a new person to Ethernet, i try to configured as a client (on STM32F429 controller) ,Initialization is done ,i ping from Command promta on LAP top, and got a response from controller. Basic communication is done...
I don't want how to send a data from client to server using server URL(I don't have IP address, i have a URL),
i send a data from client to cloud server.
please help me, i struck with last 15 day's...I waiting your reply....
Thanks in advance.
2017-06-22 8:04 AM
This is not related to STM32 at all, and only marginally related to W5500. You need to gain a deeper understanding of Internet and its protocols suite first.
URL is resolved into IP address using DNS.
Wiznet has some sort of a
http://wizwiki.net/wiki/doku.php?id=products:w5500:driver&s[]=dns
, but I am not going to investigate this for you.JW
2017-06-22 7:29 PM
hi,
Do you mean your w5500 is working as a HTTP Client?
You need to test your DNS first!
First you need to choose a DNS server for requesting, for example 8.8.8.8 is Google's DNS server.
Check the ioLibrary, there are dns.c and dnc.h files
Just call the routine:
/*
* @brief DNS process * @details Send DNS query and receive DNS response * @param dns_ip : DNS server ip * @param name : Domain name to be queryed * @param ip_from_dns : IP address from DNS server * @return -1 : failed. @ref MAX_DOMIN_NAME is too small \n * 0 : failed (Timeout or Parse error)\n * 1 : success * @note This funtion blocks until success or fail. max time = @ref MAX_DNS_RETRY * @ref DNS_WAIT_TIME */int8_t DNS_run(uint8_t * dns_ip, uint8_t * name, uint8_t * ip_from_dns);
Indeed, your question really has little to do with STM32!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.