2013-11-05 8:21 AM
Recently I had a chance to do some quick ESD tests on my board, unfortunately time was very limited.
Some basic information: -STM32F103T8U6 MCU, -USB bus powered, -USB is already protected with USBLC6-2SC6, -Plastic enclosure (almost entirely occupied by PCB), -no other connectors beside USB plug, no buttons / LEDs -PCB space is very limited, For 2kV and 4kV air-discharge everything was just fine. At 8kV my device stopped working. At first, after reset (unplug & plug) everything was back to normal, however after several attempts, I ended up with 2 dead boards. It turns out that in both cases only part that failed was the MCU. 1) How should I configure unused IO pins (power consumption is not important)? 2) What should I do with QFN pad? Currently it is left unconnected. Should I connect it to GND? 3) What about USB shield? I think about making a ''guard-ring'' along PCB edges, directly connected to USB shield, which will be connected to GND at a single point (via 4.7nF capacitor and 1M ohm resistor or alternatively via 0 ohm resistors). I would also be very interested in any other tips/suggestions. #esd2013-11-08 3:43 AM
I'd start by checking the decoupling on the power supply. Normally when you start popping devices its due to an over-voltage on the supply caused by the ESD strike; you need to shunt the energy to ground otherwise you can induce latchup. I found 100nf in parallel with 1nf was a good combination in sorting this type of problem.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.