2020-05-28 3:07 AM
Hello
II've been working on Host SMBus mode using STM32F417 and HAL F4 version 1.25.
When debugging errors on bus I found next code in function SMBUS_MasterTransmit_BTF (file stm32f4xx_hal_smbus.c line 2020).
/* Call TxCpltCallback() directly if no stop mode is set */
if (((CurrentXferOptions != SMBUS_FIRST_AND_LAST_FRAME_NO_PEC) || (CurrentXferOptions != SMBUS_FIRST_AND_LAST_FRAME_WITH_PEC)) && ((CurrentXferOptions != SMBUS_LAST_FRAME_NO_PEC) || (CurrentXferOptions != SMBUS_LAST_FRAME_WITH_PEC)) && (CurrentXferOptions != SMBUS_NO_OPTION_FRAME))
{
__HAL_SMBUS_DISABLE_IT(hsmbus, SMBUS_IT_EVT | SMBUS_IT_BUF | SMBUS_IT_ERR);
hsmbus->PreviousState = SMBUS_STATE_MASTER_BUSY_TX;
hsmbus->Mode = HAL_SMBUS_MODE_NONE;
hsmbus->State = HAL_SMBUS_STATE_READY;
#if (USE_HAL_SMBUS_REGISTER_CALLBACKS == 1)
hsmbus->MasterTxCpltCallback(hsmbus);
#else
HAL_SMBUS_MasterTxCpltCallback(hsmbus);
#endif /* USE_HAL_SMBUS_REGISTER_CALLBACKS */
}
else /* Generate Stop condition then Call TxCpltCallback() */
{
/* Disable EVT, BUF and ERR interrupt */
__HAL_SMBUS_DISABLE_IT(hsmbus, SMBUS_IT_EVT | SMBUS_IT_BUF | SMBUS_IT_ERR);
/* Generate Stop */
SET_BIT(hsmbus->Instance->CR1, I2C_CR1_STOP);
hsmbus->PreviousState = HAL_SMBUS_STATE_READY;
hsmbus->State = HAL_SMBUS_STATE_READY;
hsmbus->Mode = HAL_SMBUS_MODE_NONE;
#if (USE_HAL_SMBUS_REGISTER_CALLBACKS == 1)
hsmbus->MasterTxCpltCallback(hsmbus);
#else
HAL_SMBUS_MasterTxCpltCallback(hsmbus);
#endif /* USE_HAL_SMBUS_REGISTER_CALLBACKS */
}In my opinion condition in test CurrentXferOptions (in line 1 in snippet) is always true. And no Stop generated when last frame is detected.
I am right please?
Similar situation is in function SMBUS_MasterTransmit_TXE.
I found one small error calling two times same handler. ( function SMBUS_ITError )
/* Call user error callback */
HAL_SMBUS_ErrorCallback(hsmbus);
#if (USE_HAL_SMBUS_REGISTER_CALLBACKS == 1)
hsmbus->ErrorCallback(hsmbus);
#else
HAL_SMBUS_ErrorCallback(hsmbus);
#endif /* USE_HAL_SMBUS_REGISTER_CALLBACKS */With regards
Ivan
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.