2024-10-10 4:43 AM
Status bits in the RCC internal clock source calibration register (RCC_ICSCR) indicate which clock(s) is (are) ready and which clock is currently used as a system clock.
Should be the following:
Status bits in the RCC clock control register (RCC_CR) indicate which clock(s) is (are) ready.
Status bits in the RCC clock configuration register (RCC_CFGR) indicate which clock is currently used as a system clock.
Solved! Go to Solution.
2024-10-10 7:12 AM
Hello @MorganG ,
I confirm the issue, the link and the content will be changed. Thanks for spotting and reporting it. This will be fixed for the next document revision.
Best regards,
Simon
2024-10-10 6:35 AM - edited 2024-10-10 7:21 AM
Hello @MorganG and welcome to the Community,
Thank you for raising this issue.
I will check this and will get back to you soon with update (Internal ticket is submitted ID 193408 - not available outside of ST)
2024-10-10 7:12 AM
Hello @MorganG ,
I confirm the issue, the link and the content will be changed. Thanks for spotting and reporting it. This will be fixed for the next document revision.
Best regards,
Simon
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.