2012-11-29 4:48 AM
I'm trying to read the tow signals from the encoder quadrature . I work with COIDE of coocox. but I don't know how i should write in the Default_handler (IRQ_TIM3).
I want read the both edges of the encoder signals,and know the value of my counter timer. 1) I ask if my configuration are OK ? 2) how i write in the IRQ of ''startup_stm32f10x_md_vl.c'' in encoder.c I write : &sharpinclude ''stm32f10x.h'' &sharpinclude ''encodeur.h'' void config(void){ TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure; TIM_ICInitTypeDef TIM_ICInitStructure; GPIO_InitTypeDef GPIO_InitStructure_Encoder; /* Enable TIMER GPIO clocks */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA | RCC_APB2Periph_AFIO, ENABLE); RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM3,ENABLE); GPIO_InitStructure_Encoder.GPIO_Pin = GPIO_Pin_6 | GPIO_Pin_7; GPIO_InitStructure_Encoder.GPIO_Mode = GPIO_Mode_IN_FLOATING; GPIO_InitStructure_Encoder.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOB,&GPIO_InitStructure_Encoder); /* Timer configuration in Encoder mode */ TIM_DeInit(ENCODER_TIM); TIM_TimeBaseStructure.TIM_Prescaler = 0; // No prescaling TIM_TimeBaseStructure.TIM_Period = ENCODER_TIM_PERIOD-1; TIM_TimeBaseStructure.TIM_ClockDivision = TIM_CKD_DIV1; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseInit(ENCODER_TIM, &TIM_TimeBaseStructure); TIM_EncoderInterfaceConfig(ENCODER_TIM, TIM_EncoderMode_TI12,TIM_ICPolarity_Rising, TIM_ICPolarity_Falling); TIM_ICStructInit(&TIM_ICInitStructure); TIM_ICInitStructure.TIM_ICFilter = ENC_FILTER;//ICx_FILTER; TIM_ICInit(ENCODER_TIM, &TIM_ICInitStructure); ENCODER_TIM->CNT = 0; TIM_Cmd(ENCODER_TIM, ENABLE); } int main(void){ void config(void); } ________________ in the ''startup_stm32f10x_md_vl.c'' i write // configuration static void Default_Handler(void) { /* Go into an infinite loop. */ while (1) { int curCount= ENCODER_TIM->CNT; // i juste added this line in this file }} #enoder-interface-handler2012-11-30 12:15 PM
He's using TIM_GetCounter(TIM4); aka TIM4->CNT
It's a single register, it should be pretty apparent if it's counting up or down, or not. Sit in a loop and see if it changes and printf() the new value, and repeat.2012-11-30 1:39 PM
2012-11-30 2:39 PM
On the F1 series, input pulled up is
GPIO_InitStructure_Encoder.GPIO_Mode = GPIO_Mode_IPU;2012-12-01 3:46 AM
Here the working reading routine:
// Fir Selection public __IO FirSelection fs; static void UiDriverUpdateFirSelection(void) { fs.value_new = TIM_GetCounter(TIM4); // Ignore lower value flickr if(fs.value_new < ENCODER_FLICKR_BAND) return; // Ignore higher value flickr if(fs.value_new > (FIR_ENCODER_RANGE/FIR_ENCODER_LOG_D) + ENCODER_FLICKR_BAND) return; // No change, return if(fs.value_old == fs.value_new) return; //printf(''fir pot: %d\n\r'',fs.value_new); // Update filter control_whatever(ag.value_new - ENCODER_FLICKR_BAND); // Updated fs.value_old = fs.value_new; } void main() { // Init FIR pot fs.value_old = 0; fs.value_new = FIR_ENCODER_RANGE; while(1) { UiDriverUpdateFirSelection(); } } // Protective band on top and bottom scale // dependent on encoder quality and debounce // capacitors #define ENCODER_FLICKR_BAND 3 // -------------------------------- // Maximum pot value #define FIR_ENCODER_RANGE 10 // Divider to create non linearity #define FIR_ENCODER_LOG_D 1 // FIR selector public structure typedef struct FirSelection { // pot values // ulong value_old; // previous value ulong value_new; // most current value } FirSelection; So your controlled function will get a value from 0 - 10 based on encoder position. When max value is reached - no call to the function will be send, same for lowest position. Hope this helps.2012-12-01 5:08 AM
so i will change the mode ..i found IPU mode and i will test again
2014-12-03 7:47 AM
@wolf_man
Can you put your final code here, Please?2014-12-03 10:49 AM
This is a two year old thread, start a new one, state your specific situation, and pin connectivity. I know I've posted several, working, encode mode examples here on the forum.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.