2010-06-22 6:17 PM
Eclipse gdb error 'Don't know how to run. Try 'help target' '
2011-05-17 4:55 AM
A google search for this error indicates an issue with gdb when pathnames have a space. This does not seem to be the case here as both projects are in the same Projects folder.
2011-05-17 4:55 AM
In regard to warning; ''not enough working area available(requested 8192, free 8144)''
The following post explains that this is expected because flash algorithm uses 48 bytes.http://www.mail-archive.com/openocd-development@lists.berlios.de/msg03600.html
2011-05-17 4:55 AM
I found that the gdb run command was not complete, my cut and paste error. Now updated to the following;
target remote localhost:3333symbol-file main.out
monitor soft_reset_halt
monitor flash erase_sector 0 0 31
monitor flash write_image main.bin 0x08000000
thbreak main
cont
I no longer get the original error and gdb seems to keep running. Looks like I may have a program error as it goes to the hardfault handler with gdb console;Info: server.c:78 add_connection(): accepting 'gdb' connection from 0
Warning: gdb_server.c:416 gdb_get_packet_inner(): acknowledgment received, but no packet pending
User: target.c:1838 handle_soft_reset_halt_command(): requesting target halt and executing a soft reset
User: gdb_server.c:574 gdb_output(): erased sectors 0 through 31 on flash bank 0 in 1.029602s
Warning: target.c:853 target_alloc_working_area(): not enough working area available(requested 8192, free 8144)
User: gdb_server.c:574 gdb_output(): wrote 11262 byte from file main.bin in 1.451803s (7.575440 kb/s)
Error: cortex_swjdp.c:222 swjdp_transaction_endcheck(): SWJ-DP STICKY ERROR
Error: cortex_swjdp.c:236 swjdp_transaction_endcheck(): dcb_dhcsr 0x30003, nvic_shcsr 0x20000, nvic_cfsr 0x1, nvic_bfar 0xe000edf8
Error: cortex_swjdp.c:222 swjdp_transaction_endcheck(): SWJ-DP STICKY ERROR
Error: cortex_swjdp.c:236 swjdp_transaction_endcheck(): dcb_dhcsr 0x30003, nvic_shcsr 0x20000, nvic_cfsr 0x1, nvic_bfar 0xe000edf8
Warning: cortex_swjdp.c:703 ahbap_read_buf_u32(): Block read error address 0xfffffff0, count 0x1
Error: gdb_server.c:1024 gdb_error(): unexpected error -107 Now need to decipher the above error....
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.