2009-10-07 1:30 AM
Double Buffering on Interrupt Endpoint Issue
2011-05-17 4:25 AM
Hi,
I am trying to implement Double Buffering on Interrupt Endpoint. For initializing i am using the following code /* Initialize Endpoint 1 */ SetEPType(ENDP1, EP_INTERRUPT); SetEPDblBuffAddr(ENDP1,ENDP1_BUF0Addr,ENDP1_BUF1Addr); ClearDTOG_RX(ENDP1); ClearDTOG_TX(ENDP1); SetEPTxStatus(ENDP1, EP_TX_VALID); SetEPRxStatus(ENDP1, EP_RX_DIS); SetEPTxStatus(ENDP1, EP_TX_NAK); For sending i am using the following code void HID_SendData(uint8_t *buffer, uint32_t length) { uint32_t Endpoint_DTOG_Status = _GetENDPOINT(ENDP1) & EP_DTOG_TX; //Double buffered send. if(length) { SetEPDblBuffCount(ENDP1, EP_DBUF_IN, length); if (!Endpoint_DTOG_Status) { UserToPMABufferCopy(buffer,ENDP1_BUF0Addr, length); } else { UserToPMABufferCopy(buffer,ENDP1_BUF1Addr, length); } FreeUserBuffer(ENDP1, EP_DBUF_IN); SetEPTxCount(ENDP1,length); SetEPTxValid(ENDP1); } } The issue is always the data in the first buffer is sent to the Host, even though the filling of the second buffer is happening with the above send routine. The two buffer addresses were give as follows #define ENDP1_BUF0Addr (0x100) #define ENDP1_BUF1Addr (0x140) Please let me know if i am doing anything wrong in the intialization or sending. Thanks Siva2011-05-17 4:25 AM
Got a reply from the Index>>USB Forum.
Here is the reply http://www.st.com/mcu/forums-cat-8985-12.html Thanks SivaWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.