2018-09-05 7:52 PM
Sorry for weird English
I try use SysTick_Handler in LL library (with STM32L011F4U and CubeMX ), but never execute the Handler.
I also tried HAL library, then executed properly.
So I checked difference between HAL and LL , and I recognized initializing function in LL library ((stm32l0 xx_ll_utils.h as below) don't write [SysTick_CTRL_TICKINT_Msk] .
__STATIC_INLINE void LL_InitTick(uint32_t HCLKFrequency, uint32_t Ticks)
{
/* Configure the SysTick to have interrupt in 1ms time base */
SysTick->LOAD = (uint32_t)((HCLKFrequency / Ticks) - 1UL); /* set reload register */
SysTick->VAL = 0UL; /* Load the SysTick Counter Value */
SysTick->CTRL = SysTick_CTRL_CLKSOURCE_Msk |
SysTick_CTRL_ENABLE_Msk; /* Enable the Systick Timer */
}So I modified as below then executed SysTick_Handler() properly.
__STATIC_INLINE void LL_InitTick(uint32_t HCLKFrequency, uint32_t Ticks)
{
/* Configure the SysTick to have interrupt in 1ms time base */
SysTick->LOAD = (uint32_t)((HCLKFrequency / Ticks) - 1UL); /* set reload register */
SysTick->VAL = 0UL; /* Load the SysTick Counter Value */
SysTick->CTRL = SysTick_CTRL_CLKSOURCE_Msk |
SysTick_CTRL_TICKINT_Msk | /* Enable the Systick Interrupt */
SysTick_CTRL_ENABLE_Msk; /* Enable the Systick Timer */
}On CubeMX, enable Systick interrupt as default ( and can't disable)
Is this LL library's bug ?
if so , I want to fix this by ST.
Please tell me your opinion.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.