2021-11-14 6:19 AM
I can not start transfer via SWO to STM32H743.
Port PB3 initialized clock feed.
Initialized SWO:
*(__IO uint32_t*)(0x5C001004) |= 0x00700000; // DBGMCU_CR D3DBGCKEN D1DBGCKEN TRACECLKEN
//UNLOCK FUNNEL
*(__IO uint32_t*)(0x5C004FB0) = 0xC5ACCE55; // SWTF_LAR
*(__IO uint32_t*)(0x5C003FB0) = 0xC5ACCE55; // SWO_LAR
//SWO current output divisor register
//This divisor value (0x000000C7) corresponds to 400Mhz
//To change it, you can use the following rule
// value = (CPU Freq/sw speed )-1
*(__IO uint32_t*)(0x5C003010) = ((SystemCoreClock / 2000000) - 1); // SWO_CODR
//SWO selected pin protocol register
*(__IO uint32_t*)(0x5C0030F0) = 0x00000002; // SWO_SPPR
//Enable ITM input of SWO trace funnel
*(__IO uint32_t*)(0x5C004000) |= 0x00000001; // SWFT_CTRL
// Configure GPIOB pin 3 as AF
*(__IO uint32_t*)(0x58020400) = (*(__IO uint32_t*)(0x58020400) & 0xffffff3f) | 0x00000080;
// Configure GPIOB pin 3 Speed
*(__IO uint32_t*)(0x58020408) |= 0x00000080;
// Force AF0 for GPIOB pin 3
*(__IO uint32_t*)(0x58020420) &= 0xFFFF0FFF;
uint32_t SystemCoreClock = 480000000;include printf:
int _write ( int file, char *ptr, int len )
{
int i = 0;
for ( i = 0; i < len; i++ )
ITM_SendChar ( *ptr++ );
return len;
}Calls when passing a message through printf (); Checked set the brepoint in _write the moment the transfer is called
I checked the PB3 leg with an oscilloscope there is no signal. The call to _write is passed to ITM_SendChar (* ptr ++); there is.
What is the matter, I ask for help.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.