2026-01-02 1:17 PM - edited 2026-01-02 1:36 PM
I am using two UARTs simultaneously.
The CPU is STM32H743. One UART is on UART 4 that transmits information to pc uart
And the other UART on UART 5 receives information from pc
If these UARTS function alone, they function well.
I am using the DMA idle function on the receive and the DMA function on the transmit
When they function together, the information is not properly received from the PC on UART 5.
Please help me resolve this issue
2026-01-02 2:49 PM
Multiple UARTs can work together at the same time. They are independent.
It's going to be hard to debug without seeing any code.
2026-01-03 2:13 AM
As @TDK said, there's no inherent reason why multiple UARTs can't work simultaneously - so it must be something in your hardware and/or software setup.
Therefore, you'll need to give details of your hardware and software setup.
See: How to write your question to maximize your chances to find a solution
And: How to insert source code
@dorong wrote:the information is not properly received from the PC on UART 5.
So UART4 remains fine?
What, exactly, does "not properly received" mean?
@dorong wrote:One UART is on UART 4 that transmits information to pc uart
And the other UART on UART 5 receives information from pc
Is there a particular reason for using two separate UARTs - one for transmit, and another for receive?
UART = Universal Asynchronous Receiver and Transmitter - one UART can do both receive and transmit!
How are these UARTs connected to the PC ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.