2023-04-04 1:19 PM
What are the main differences between using C and C++ for STM32 microcontroller programming? Which language is better suited for different use cases, and what are some factors to consider when choosing between the two for embedded system development?
2023-04-04 2:12 PM
Sounds like a homework question..
C++ can be bulkier, and has more demands on dynamic memory allocation.
C++ hides complexity, C forces you to account for it and own it.
C facilitates a lot of bad programmers, with poor habits, C++ forces a more structured and object orientated approach.
Not all people using C have a million global variables with subtly different unique names.
If you can't determine which is suitable for your use case, you probably need more experience.
2023-04-04 7:46 PM
C language is still the most common programming language for embedded microcontrollers.
(beyond embedded, C is still popular, at least by TIOBE index TIOBE Index - TIOBE
The C language spec has evolved, yet compiler adoption to the upgrades takes time.
Comments with "//" is one example.
Most of C++ improvements can be coded in C with less readability (structure with function pointers members....).
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.